Bauma 2016

MTU Onsite Energy to showcase gensets for construction sites at Bauma

Posted on 19 January 2016 by Yvonne Wirth, Images by MTU Onsite Energy

MTU Onsite Energy will be presenting mobile and stationary diesel gensets at Bauma.

MTU Onsite Energy will be presenting mobile and stationary diesel gensets at Bauma, that are ideally suited to the generation of electric power on construction sites. The Bauma trade fair for construction machinery takes place from 11 to 17 April 2016 in Munich. On stand 314 in Hall A4, the company will also be presenting MTU engines for construction site vehicles.

A model of a 20-foot container genset that has been included in the MTU Onsite Energy product portfolio since 2015 will also be on show. Based on the new generation of Series 2000 engines, the genset is fitted with a common rail injection system. The Series 2000 engines are designed to cover an output range of up to 1,400 kVA for standby power and deliver up to 1.250 kVA prime power. As a result of its modular design, the 20-foot container genset can be used in a wide variety of applications and is ideally suited to rugged operating conditions and operation in remote areas. It is provided with a two-door system, which provides access to all components for maintenance purposes.

The MTU Onsite Energy portfolio includes generator sets and container gensets in a power range extending from 30 to 3,250 kWe.

Point of Contact

Ralf Patschke
Tel.:
+49 7541 90 2589
E-mail:

Related stories

MTU to showcase EU Stage V engines for construction equipment at Bauma

by Silke Rockenstein

MTU will be presenting its engines for the off-highway emission regulations expected to come into force as of 2019 to the construction industry at BAUMA.

Read more

50 degrees and no shade

by Yvonne Wirth

Gensets based on MTU engines provide a camp in the Australian outback with a reliable power supply.

Read more