Construction & Industrial

MTU moves into excavator market with engines for JCB

Posted on 06 February 2017 by Silke Rockenstein, Images by JCB; MTU

MTU 6R 1000 engines for JCB’s new JS 300, 330 and 370 excavators

For the first time, MTU will be supplying engines for use in excavators, having won an order from British construction equipment manufacturer JCB. MTU’s Series 1000 engines are compliant with EU-Stage IV and EPA Tier 4f emissions legislation and are to be used to power new excavators in JCB’s JS 300, JS 330 and JS 370 series. The construction machinery manufacturer is choosing MTU for its excavators for the first time. MTU has been supplying Series 4000 engines for huge mining excavators of different manufacturers for decades.

The excavators weigh between 30 and 37 tonnes and each is to be powered by a 6-cylinder Series 1000 inline engine from MTU delivering up to 210 kW. Also driven by MTU Series 1000 units is JCB’s new 457 wheel loader, which was launched on the market two years ago.

MTU 6R 1000 engines for JCB’s new JS 300, 330 and 370 excavators

Tim Burnhope, JCB Chief Innovation and Growth Officer, said: “JCB already uses MTU engines in its flagship 457 wheeled loaders. The introduction of the engine into three of our JS excavators will offer customers fuel savings of up to 10%.”

Bernd Krüper, Vice President Industrial Business including Construction & Agriculture at MTU added, “Use of our engines in JCB's new excavators marks our entry into another very important and high-volume segment of the C&I market, and we are very proud that JCB is choosing to endorse our EU Stage IV-compliant units. This is another step forward in our long and successful partnership.”

A new JS 370 excavator equipped with an MTU 6R 1000 unit is to be unveiled at the Conexpo trade show in Las Vegas in March.

The introduction of the MTU engine into three of JCB's JS excavators will offer operators fuel savings of up to 10%. In the picture the JS 2330.


Point of Contact

Edwin de Heij
Tel.:
+31 78 63957 03
E-mail:

Related stories

Rolls-Royce delivers first Stage V MTU engines for Bell dump trucks

by Rebecca Weiand-Schütt

Bell Equipment recently received the first six EU Stage V certified Series 1000 – 1500 MTU engines from Rolls-Royce.

Read more

Certified for Stage V

by Katharina Dietrich

MTU Series 1000, 1100, 1300 and 1500 engines have been awarded their EU Stage V compliance certificates.

Read more

Tier 4-Final MTU Engines Power Growing Oil-Free Air Compressor Fleet

by Bryan Mangum

Aggreko is a global specialty rental company that supplies Power, Temperature Control and Oil-Free Compressor technologies to various industries around the world.

Read more