Railcars

First hybrid rail project in the UK

Posted on 19 September 2018 by Rolf Behrens, Images by MTU, Porterbrook

MTU and Porterbrook have agreed the delivery of MTU Hybrid PowerPacks that can convert from diesel-only to hybrid-electric operation.

MTU and Porterbrook, the UK’s largest owner of passenger rolling stock, have agreed the delivery of MTU Hybrid PowerPacks that can convert Class 168 and Class 170 ‘Turbostar’ DMUs from diesel-only to hybrid-electric operation. Hybrid technology allows for the cleaner and quieter operation of trains in stations and through urban areas.

The Letter of Intent, which was signed at rail industry trade show Innotrans, covers the delivery of hybrid systems for installation on two test trains. Following trials, Porterbrook aims to offer hybrid conversion to a range of customers operating existing Turbostar fleets. 

This is the first agreement for the delivery of MTU hybrid drive systems in the UK. 

Mary Grant, CEO of Porterbrook, said: “Porterbrook is committed to reducing the emissions and carbon footprint of our existing diesel powered fleets. We hope our investment in this trial of MTU Hybrid PowerPacks will enable us to offer wider fleet fitment of this technology, so that our customers can reduce both emissions and operating costs, as well as improve air-quality along urban corridors. Hybrid trains have the added benefit of operating with very little sound when using battery power, offering additional benefits to the railway’s near neighbours.

“This is one of several initiatives that Porterbrook is undertaking to address the challenge, set by Rail Minister Jo Johnson MP, of removing diesel-only trains from the UK rail network by 2040.” Warren East, CEO of Rolls-Royce said: “We are pleased to be helping to write a new chapter of environmentally friendly, quieter and more efficient rail travel in the UK. With the innovative MTU Hybrid PowerPacks, Rolls-Royce and our partner Porterbrook will be setting new standards on the UK network; helping to reduce emissions, increase fuel efficiency and improve the lives of people who live near train stations.”

Rolls-Royce will initially deliver two MTU Hybrid PowerPacks based on type 6H 1800 engines to Porterbrook. These will be fitted into a Turbostar DMU in the beginning of 2020 which will then be trialled for a period of six months during regular operations. The agreement includes an option for the retrofitting of a second DMU with two MTU Hybrid PowerPacks. Based on the performance of the Hybrid fitted units, Porterbrook hopes to offer customers the opportunity to convert their existing Turbostar fleets into HybridFLEX trains through the installation of MTU Hybrid PowerPacks. 

The MTU Hybrid PowerPack is an environmentally friendly drive system which combines the advantages of diesel and battery-powered rail traction. The version for Porterbrook incorporates an MTU diesel engine which fulfils future EU Stage V emissions regulations; plus an electric machine, which can be used either as an electric motor or generator; and an MTU EnergyPack battery system, which stores the energy recovered during braking. This enables very low-noise, emissions-free battery-only electric operation in urban areas and around stations. 

The MTU Hybrid PowerPack is an environmentally friendly drive system which combines the advantages of diesel and battery-powered rail traction.

Noise emissions in stations are cut by around 75 percent (20 dB(A)). Fuel consumption and CO2 emissions are reduced by up to 25 percent. NOx emissions can also be reduced by up to 70 percent and particulate emissions by around 90 percent. The total operating costs of rail vehicles with MTU hybrid drives are also significantly lower, and even brake pads and discs experience reduced wear due to energy recuperation during braking. As a result of the additional power of the electric machine, train operators also have the option to improve journey times through better acceleration. 

Drive systems from Rolls-Royce already play an important role in the British railway system. More than 1,100 MTU PowerPacks and engines already power railcars and locomotives across the UK and Ireland, including over 550 PowerPacks in Turbostar DMUs which are in service with seven operators.  

The content of the stories reflects the status as of the respective date of publication. They are not updated. Further developments are therefore not taken into account.

Point of Contact

Manfred Martin Gößler
Tel.:
+49 7541 90 7634
E-mail:

Related stories

Lifelong service

by Mirko Gutemann

MTU supplies 250 Powerpacks for new railcars in the British Intercity Express program. Maintenance contract covers next 27.5 years.

Read more

MTU Rail Power for the British Isles

by Rolf Behrens

Wherever there are tracks in the British Isles, MTU rail drive systems deliver the power for locomotives and railcars.

Read more

Time has come for the hybrids

by Lucie Maluck

MTU's hybrid traction system has established itself in the rail market - Experts comment on that.

Read more