STORY Naval Solutions

German Navy’s most modern frigate enters service with mtu power

Posted on June 19, 2019 by Rolf Behrens, Images by Rolls-Royce Power Systems, thyssenkrupp Marine Systems

Frigate „Baden-Württemberg“ has just entered service. mtu propulsion and automation technologies play a decisive role for its success.
Wilhelmshaven, Germany

Frigate „Baden-Württemberg“, the most modern vessel of the German Navy, has just entered service. German federal minister of Defense, Ursula von der Leyen, attended the handover ceremony of the new vessel which bears the name of the German federal state from which core components of its propulsion system derive: Propulsion and automation technologies from mtu play a decisive role for the service and success of the frigates of the new F125 class and enable the new intensive use concept of the German Navy for these vessels. The ships can remain in operation for up two years without interruption, only the crew will be exchanged each four months. This is possible only thanks to the reliability of mtu engines and the cutting-edge mtu automation system Callosum which allows for example for the maintenance of engine on board of the ships. 

The commissioning ceremony took place at the naval base of Wilhelmshaven in northern Germany. (Picture: thyssenkrupp Marine Systems)

For the Class F125 frigates, mtu delivers diesel gensets and gas turbine modules which are a crucial part of the ships’ combined diesel-electric and gas turbine (CODLAG) propulsion system. Four gensets based on 20V 4000 M53B engines each producing 3,015 kW of mechanical output generate the electric power both for diesel-electric propulsion for cruising speeds of up to 20 knots and for the on-board power supply system. The four diesel engines are switched on or off sequentially depending on the power required so that they can be operated within their optimum range. That spares the engines and reduces fuel consumption. Major overhaul is only needed after five years of operation. This represents a quadrupling of the maintenance intervals as compared to previous classes of frigates.

The mtu gensets are encapsulated by acoustic enclosures in order to keep the frigates’ acoustic signature extremely low.

During maintenance technicians receive support from mtu-developed automation system Callosum MT: The service and maintenance system constantly monitors all engine-related processes. If a malfunction occurs or a routine maintenance task is due, the system informs the relevant personnel immediately and in a very precise manner. The system does not only show where a malfunction occurred but also guides the mechanics through each step of repair, giving exact information on which tools, spare parts and consumables are needed. The technicians can also view a 3D video on the mtu station installed in the engine room, explaining how to carry out the repair. 

The second vessel of class F125, called “Nordrhein-Westfalen”, is set to enter service later this year. A further two of these frigates with propulsion and automation technology from mtu are to be delivered within the next two years. 


Point of contact

Giovanni Spadaro
Phone:
+49 7541 90 4063
+49(0)7541 904063
Fax:
+49(0)7541 90904063
E-mail:

Related stories

Naval Solutions

mtu Virtual Marine Symposium provides impulses for the climate-friendly transformation of shipping

Read more

Naval Solutions

Systems Solutions for Naval Vessels

mtu solutions are dedicated to innovative thinking and providing the perfect engines and systems for your fleet as it secures the seas. mtu engines and propulsion systems are playing an important role of many countries’ armed forces. For more than half a century, we have been as much at home on the sea as you are. It is this experience and expertise that makes us such a strong partner – worldwide, whatever mission you are on.

Read more

Yacht

Trade show highlights on the Mediterranean

by Katrin Auernhammer

In Cannes and Monaco, many yacht innovations will be lined up in September. It's all about design, size and propulsion. We feature some yachts with mtu engines.

Read more