Power Generation

Rolls-Royce subsidary mtu supplies ten emergency diesel gensets to nuclear power plant in Belarus

Posted on 20 November 2014 by Silke Rockenstein, Images by mtu Arvchive

Rolls-Royce subsidiary MTU Friedrichshafen has won an order for supplying Ostrovets 1&2, the Belarusian Nuclear Power Plant (NPP), with ten emergency diesel gensets (EDGs).

Rolls-Royce subsidiary MTU Friedrichshafen has won an order for supplying Ostrovets 1&2, the Belarusian Nuclear Power Plant (NPP), with ten emergency diesel gensets (EDGs). The customer is mtu’s long term partner in this segment, general contractor Zvezda Energetika from St. Petersburg in Russia. The deal is worth several tens of millions of Euros.

Each genset delivers an electrical power output of 6,300 kW. These are the most powerful gensets in mtu's portfolio and are based on its latest high-speed 20V 956 TB34 engines, whose output is almost 5% higher than the previous version. mtu is part of Rolls-Royce Power Systems within the Land & Sea division of Rolls-Royce.

The first nuclear power plant in Belarus is being built by ROSATOM, the Russian state atomic energy corporation, and is to start commercial operation from 2018. With this plant, Belarus intends to reduce the country's dependence on energy imports. The gensets are to be supplied in 2016 and 2017 for the plant's two pressurized-water reactors VVER 1200.

“We are honoured that the ROSATOM atomic energy corporation trusts our technological expertise,” said Dr Michael Haidinger, CSO at Rolls-Royce Power Systems. “We see this contract as confirming us as the leading foreign supplier of emergency diesel gensets for ROSATOM and consolidating our market leadership position in the EDGs market for VVER reactors.”

mtu has successfully taken part in numerous projects involving the supply of emergency diesel gensets to nuclear power plants with VVER reactors in the last few years. These include Tianwan 1&2 and 3&4 in China, Novovoronezh II 1&2 in Russia and Mochovce 3&4 in Slovakia. 

Point of Contact

Aleksandr Morozov
Tel.:
+49 821 7480 2321
E-mail:

Related stories

Power Generation

mtu safeguards continuous emergency operation at Kårstø natural gas processing plant

The Norwegian natural gas processing plant at Kårstø has been equipped with a new emergency power system as part of a long-term expansion project. During any future power outages, five mtu gensets powered by Type 16V 4000 G63 engines will be in place to supply the energy for essential production processes — and, thanks to special acoustic technology, they will do their job more quietly than ever.

Read more

Power Generation

GenDrive Engines

With reliable and proven mtu genset engines, you benefit from over half a century of experience in the production of drive systems for diesel gensets.

Read more

Power Generation

EMERGENCY BACKUP SOLUTION FOR ADELAIDE’S FLAGSHIP HOSPITAL

The $2.3 billion Royal Adelaide Hospital has been listed as the single largest capital investment project in the history of South Australia. Built to the world’s best standards, it is the state’s flagship hospital, providing a comprehensive range of the most complex clinical care for the people of South Australia. To deliver emergency power to the all-new hospital, the local mtu partner Penske Power Systems has supplied and managed the installation of six diesel-powered mtu 20V 4000 DS 2650 generators. 

Read more