On the way to NetZero: mtu fuel cell solutions

Making drives, propulsion and power generation CO2-free.

Wouldn't it be wonderful if we could produce driving power and energy and stay climate-neutral at the same time? And do that right across the globe – from the remotest corners of the earth to the megacities?

mtu fuel cell solutions of the future are set to turn that vision into reality. Fuel cells produce clean electrical power. Fuel cells can run on green hydrogen. Fuel cells emit steam and a little bit of heat – nothing more. That's why we're looking forward to a CO2-free future.  

Spot on: mtu fuel cell solutions

Youtube Video

Electrical power from hydrogen and oxygen – how fuel cells are used in power generation

The Rolls-Royce business unit Power Systems is developing complete and fully integrated mtu fuel cell solutions for the reliable generation of continuous and prime power in the MW range. And because they can be deployed as flexibly as a diesel engine, complete fuel cell solutions are set to play a prominent role in the energy revolution. When they run on green hydrogen, fuel cells are capable of CO2-free and therefore climate-neutral production of electrical power. Operators in particular of data centers, which are highly energy-intensive because all the world's internet traffic passes through them, have a vested interest in reducing their CO2 footprint and thereby their impact on the world climate. And fuel cell generators – which can be deployed for emergency power – enable them to do so. In principle, we are also working on fuel cell systems for peak and continuous power supply. Their use in airports and hospitals is likewise planned. Fuel cells can also play a major role in microgrids, thereby promoting the set-up of autonomous, C02-neutral power grids all around the world.

mtu fuel cells and CO2-free mobility

In the future, mtu fuel cells are also to be used to power ships and heavy-duty off-highway vehicles. Using hydrogen and oxygen, the fuel cell produces electricity to power electric motors. Fuel cells that do so using green hydrogen are not only entirely carbon-free but highly flexible too. That is owing to another huge advantage of the fuel cell system:   its scalability. On a ship, for example, the amount of power being generated can be adapted to its power requirement at any one time, thereby saving fuel. When a lot of power is required, all fuel cells are used. When the power demand is average, fewer fuel cells are switched in. And although this technology is not yet available as standard, the way ahead to achieving that goal is clear.  

How fuel cells work

In fuel cells, hydrogen reacts with oxygen to form water, giving off electrical energy and heat in the process. A single fuel cell consists of an anode, electrolyte and a cathode. On the anode side, a catalyst splits hydrogen into hydrogen protons (H+) and electrons (e-). The protons migrate through the electrolyte to the cathode where they combine with the electrons and ambient oxygen to form water. To achieve more  power, several cells are usually connected to form a stack.

Net Zero at Power Systems

By 2050, we want to be climate neutral. With our "Net Zero at Rolls-Royce Power Systems" program, we are showing the way there.

On the way to climate neutrality - fuel cell technology for future energy and drive systems

In a white paper, Rolls-Royce Power Systems experts explain how fuel cells work and how they can be integrated into future energy and drive systems.

Need help finding the perfect product or system?

No problem at all. Let one of our expert advisors point you in the right direction.

PRESS RELEASE Corporate

Rolls-Royce-Power-Systems sets out road map for climate-neutrality with ‘Net Zero at Power Systems’ - Major reduction in emissions by 2030

Read more

STORY

How does shipping go green?

by Lucie Maluck

Read more

STORY Power Generation

Fuel cells and the quest for green power

by Lucie Maluck

Read more

STORY Power Generation

“There's simply no alternative to the Paris climate agreement”

by Kerstin Hansmann