Corporate

Net Zero at Power Systems

Our mission is climate neutrality by 2050. 'Net Zero at Power Systems' plots the way ahead.

Our way to Net Zero

The biggest threat to humanity is climate change. It is our mission to join the fight against it. That is why we are clearly committed to the Paris Climate Agreement and its goal of reducing global warming to well below two degrees Celsius with efforts to limit it to 1.5 degrees Celsius compared to the pre-industrial era through climate action. To that end, we have not only established 'Sustainable Power Solutions', our new business division tasked with building a sustainable future in the field of energy, drives and marine propulsion, but have also launched an ambitious new program - 'Net Zero at Power Systems'. In this program, one focus is gearing our product portfolio towards greater sustainability, since the biggest potential for reducing greenhouse gas emissions lies with our products.

In total, the Power Systems products sold in 2019, the year before the pandemic, will generate some 109 million tons of greenhouse gases over their service life in the field – almost double that emitted by the Greater London region every year. Our goal is to achieve a 35% decrease compared to 2019 in the greenhouse gases emitted by newly sold products. Our ultimate goal is climate-neutrality by 2050. With the same spirit we are also setting milestones for gearing our production and value chain to long-term climate neutrality. To accomplish these missions, we will be working closely with our parent company Rolls-Royce and will let ourselves be guided by the 'Science-Based-Targets' initiative.

On the way to Net Zero: We recognize in all our products great potential for reducing greenhouse gas emissions – be it by means of electrification, hybridization, system integration or alternative fuels. 

What our experts say

We want to show that active climate protection and business growth can go hand in hand

“We want to show that climate action and business growth can go hand-in-hand.” 

CEO Andreas Schell explains how Rolls-Royce
Power Systems can accomplish Net Zero through a combination of new and proven
technologies. 

Our Milestones on the Road to NetZero

"Our Milestones on the Road to Net Zero."
 

COO Dr Otto Preiss explains the steps to be
taken by Rolls-Royce Power Systems on the way to Net Zero. 

With the Green and Hightech Program, we laid the foundation for NetZero early on

"Our Green and High-Tech program formed the early foundation of today's Net Zero mission."

Dr Daniel Chatterjee, Director Technology Strategy & Regulatory Affairs at Rolls-Royce Power Systems, on the broad focus of its technology development in recent years.  

Sustainable fuels make internal combustion engines cleaner

One key to the transformation of off-highway mobility and on-site power generation lies in fuels. Modern Power-to-X technologies use green electrical power in electrolysis to produce hydrogen. Taking C02 derived from the air or biomass, this hydrogen is synthesized into E-fuels such as e-methane, e-methanol or e-diesel. Power-to-X technology makes the C02-neutral cycle possible. By 2023, our leading Series 2000 and Series 4000, which account for 85% of engine sales, will be able to run on sustainable fuels such as e- and second-generation biofuels. Some of our engines for industrial applications and for power generation can already run on e-diesel or second-generation biofuels such as HVO. In parallel, our developers are working on hydrogen and methanol engines.  

Zero emissions: Fuel cells for C02-free energy and driving power

From 2025, CO2-free fuel cell systems will form a central pillar of product strategy at Rolls-Royce Power Systems. We commissioned our first demonstration unit on our site in Friedrichshafen in 2021 already. We are planning to develop complete, scalable, integrated solutions in the megawatt range in cooperation with a cellcentric, a joint venture company set up by Daimler Truck AG and Volvo Group AB. Fuel cells will be initially deployed to feed balancing energy into the public grid to compensate fluctuations, as well to generate continuous power and provide emergency power in data centers. Subsequent extension of our fuel cell portfolio to cover marine propulsion applications is also planned. (Click here for more information.) 

Our roadmap to Net Zero

2023

From 2023, our main engine series will be ready for sustainable fuels. 

2025

From 2025 onwards, we will provide our customers with CO2-free energy supply with fuel cells.

2030

By 2030, we aim to reduce the CO2 emissions of our new products and solutions sold by 35% compared to 2019. 

2050

By 2050, the entire Rolls-Royce Group will be carbon neutral.

Foundation laid by Green and High-Tech program

Our point of departure into a climate-neutral future was the Green and Hightech Program which we launched back in 2015. To create the solutions of tomorrow, we are concentrating on alternative fuels, electrification, efficiency enhancement, system integration and digitalization. In conjunction with this program, we are investing some 500 million euros in developing sustainable technologies to build a future without fossil fuels. 

Our goal: sustainable production

Not only our products are becoming more sustainable, but also our production and our value creation chain. This year, we will also plot milestones for gearing both towards long-term climate neutrality. Since 2014, for example, we have already cut CO2 emissions by 20% at our six largest sites worldwide - through the expansion of photovoltaic systems, the increased use of combined heat and power plants, e-mobility and energy efficiency projects. But this is just the beginning. Overall, we see a CO2 savings potential of 97,000 metric tons per year. To do so will involve scrutinizing not only our own production processes and test stands, but also the unfinished products we buy, and the deployment of our products on customer sites.  

We're ready to go – join us on the journey

There was never a more exciting time in the field of energy, drives and marine propulsion. Climate-neutral mobility and power generation is possible, and will come. Even today, we offer products that generate significantly lower or virtually zero C02 emissions – mtu Hybrid PowerPacks for rail applications, for example. We are also working on mtu hybrid propulsion for marine applications. In 2018, we began producing mtu battery energy storage systems the size of freight containers that do not generate C02 emissions during operation and store electrical energy from renewable sources. Battery energy storage systems can also be integrated with microgrids and smartly connected with renewable energy systems or diesel and gas-powered generator sets, thus contributing to sustainable, off-grid power generation.The future has already begun. From now on, it's all about pulling together and continuing on this path. We look forward to working not only with our customers and partners, but with policymakers to create the conditions that will make the energy-turnaround reality.  

Our latest publications on sustainable products

Corporate

Rolls-Royce-Power-Systems sets out road map for climate-neutrality with ‘Net Zero at Power Systems’ - Major reduction in emissions by 2030

Read more

Power Generation

Fuel cells and the quest for green power

by Lucie Maluck

Fuel cells and hydrogen and methanol engines are paving the way towards sustainable power generation and off-highway mobility.

Read more

How does shipping go green?

by Lucie Maluck

E-fuels produced by Power-to-X technologies to unlock the green energy revolution in the world of shipping.

Read more

Corporate

The Future of Internal Combustion Engines as seen by Rolls-Royce Power Systems

by Dr. Otto Preiss

This white paper is intended to summarize the position of Rolls-Royce business unit Power Systems on the future of internal combustion engines (ICE) in the application areas and industries of relevance to us, including marine, industrial, and power generation applications.