Furthermore, in networks involving high numbers of PV home systems (with and without battery storage), consumers can be self-sufficient and still draw power from the grid during certain hours or in bad weather. Conventional power generation must still cover these events when large-scale storage systems are no longer an alternative due to their restricted capacity.
While combustion technologies were the heart of the power system in the past, they are now becoming a key enabler, filling the gap between demand and renewable energy production. Consequently, they facilitate the increased integration of intermittent RES into the power system, thereby accelerating the energy transition even further.
However, building up new intermittent renewable energy resources presents its own challenges. The great dependency on wind and solar energy leads to capacities being built on a large scale,
requiring vast areas to capture as much energy as possible. Point of generation and demand tend to be inherently divergent in these areas.
Large-scale renewable power plants are usually located well away from regions of high demand. Consequently, the power must be delivered to the point of demand, with an ageing transmission and distribution infrastructure struggling to integrate and bear a higher share of renewables. For example, resource availability means that wind power generation facilities are mainly situated in Scotland and offshore in the North Sea, while most heavy industry lies in the Midlands and the South of the UK. As a result, the power must be delivered to these locations, resulting in a need to extend the transmission grid, which in turn requires substantial investment to be covered by the final consumer, and also takes years to plan and build. For example, long approval times and resistance from within the population make the process lethargic, with construction and extension of the power grid often lagging behind the change in load and generation patterns.
If the grid is unable to cope with all the power injected, renewable power generation can become subject to redispatching (i.e., constraint management), while conventional power plants in high-load areas ramp up. This means that renewable power plants have to decrease their output in response to grid constraints, while conventional distributed capacities, operating independently of the weather in high-load regions, can be an alternative solution to cover renewable shortcomings and peak loads until the infrastructure has been enhanced and/or local RES generation catches up, thus lowering the need to transport RES energy over great distances.