Tognum to deliver rail drive systems for Ireland
Posted on August 04, 2009
- Expansion of systems business for rail applications
- Delivery of environmentally compatible mtu powerpacks to Rotem
- Order volume: € 11 million
Friedrichshafen, 4 August 2009. The propulsion and power solutions specialist Tognum is currently furthering a considerable expansion of their systems business in the field of rail applications. Tognum’s business unit “Engines“ has recently been awarded an order for the delivery of so-called “powerpacks” in the amount of € 11 million by Korean railcar manufacturer Rotem. From 2011, these rail drive units will be utilized in railcars to be used for operation in Irish local and regional rail traffic. Final customer is the railway operator Irish Rail and delivery of these powerpacks is scheduled between the end of 2009 and October 2010.
Tognum had been awarded an order with a volume of € 25 million for the delivery of rail powerpacks to Ireland by Rotem as early as 2005. The current follow-up order also comprises complete rail drive systems consisting of engines and other components like gear boxes, filter systems and cooling systems. The overall system is based on an environmentally compatible 6H 1800 R83 engine with a power output of 360 kW, thus complying with the stringent EU Stage IIIA exhaust gas emission standards. Not only do these powerpacks feature considerable acceleration characteristics, but also low life cycle costs as well as low noise and vibration levels.
“This order highlights our position as a leading provider of tailored complete systems for rail applications“, explains Rainer Breidenbach, member of the executive board of Tognum AG with responsibility for the business unit “Engines”. “Within our new strategic initiative ‘propulsion’, and, in order to fully prepare ourselves for future requirements, we are currently putting our focus on innovative and intelligent drive solutions like hybrid technology, for example”, Breidenbach continued.
During the past year, Tognum has launched a prototype for a diesel railcar hybrid drive system featuring exhaust gas after treatment, complying with the requirements of the EU Stage IIIB guideline, which will take effect as of 2012.
Phone: |
+49 7541 90 3989
|
E-mail: |