“Conventional coal plants are being decommissioned, while renewable generation remains intermittent,” says Pierangeli. “In addition, geopolitical instability is increasing pressure on energy security, and the load profiles of AI data centers are growing dramatically more volatile.
”It is projected that the total power generation market will nearly triple between 2025 and 2030, driven primarily by data center demand, with the backup power segment growing at approximately 22% annually and the continuous power segment growing at 24%. Yet supply is struggling to keep pace.
“Cumulative U.S. grid power supply to data centers is forecast to fall more than 50 gigawatts short of demand by 2030,” says Pierangeli. “And while a data center itself can be built in 18 to 24 months, securing a grid connection takes 3 to 7 years.”
Speed-to-market is the name of the game when it comes to the AI-race and keeping up with demand. Major hyperscalers can’t wait several years for a utility connection, which is where new opportunities are emerging, especially for our mtu gas gensets in the near term and Small Modular Reactors (SMRs), further down the line. While hyperscalers ramped up data center capital expenditure announcements by more than 50% in early 2026 alone, the utility sector is years behind.
Prime power: Bring your own
As grid constraints intensify and public push back on data center electricity consumption slow permitting of new projects, on-site power generation becomes a key enabler. Often referred to as “Bring Your Own Power” initiatives, developers are increasingly incorporating independent power plants in new data center concepts that allow them to produce the energy needed to run the facility until grid supply or new energy sources, such as nuclear, are available.
mtu gas generator systems are an excellent fit for this continuous power supply—either directly at the data center (“behind the meter”) or as part of dedicated power plants.
With short deployment times, high operational flexibility and a modular design, these systems offer high efficiency and speed-to-market that make them highly attractive for new data center projects. In places like the U.S. where natural gas is plentiful and pipelines are well established; the operational and cost implications are also very attractive.