STORY Commercial Marine

Green methanol for mtu marine engines

Posted on January 20, 2025 by Lucie Maluck, Images by Rolls-Royce Power Systems

What makes methanol such an interesting alternative for shipping? And what challenges await the Rolls-Royce engineers who are developing mtu engines for this fuel?
Sustainable mtu solutions for a green future
Internal combustion engines are an indispensable companion to the energy transition. That is why we are continuing to develop them and make them fit for climate-neutral operation.
Read more
It seems like a Herculean task: the shipping industry - an industry that burned 180 million tons of oil-equivalent fossil fuel in 2022 - wants to become climate-neutral by 2050. One key to this could lie in a simple, colorless alcohol: Methanol. It is clean, efficient and can power ships in a climate-neutral way if it is produced using green electricity. What makes methanol such an interesting alternative for shipping? And what challenges await the Rolls-Royce engineers who are developing mtu engines for this fuel? 

"Green methanol has the potential to shape the energy transition in marine propulsion systems," says Denise Kurtulus. She heads up the mtu marine propulsion business at Rolls-Royce's Power Systems division and has long been convinced that methanol can be a real game changer. Why? •

  • Sustainability: Green methanol, which is produced by synthesizing CO2 and green hydrogen, can power ships in a climate-neutral way. It is true that CO2 is released when methanol is burned, regardless of whether it is green or not. However, in the case of green methanol, the CO2 has already been removed from the air during production. In addition to e-methanol, which is produced from synthesis, this also applies to bio-methanol, which can be produced  from biomass.  The carbon cycle keeps the CO2 content of the atmosphere in balance. In addition, methanol burns cleaner than conventional fossil fuels and therefore produces less sulphur oxides, nitrogen oxides and soot particles (particulate matter). 
  • Tank volume: Methanol has only around 50 percent of the energy density of diesel. This means that the tank volume must be twice as large as that of conventional diesel engines. However, this is still the best alternative among the "green" fuels. The volume of ammonia is comparable to that of methanol, while that of hydrogen is considerably higher. 
  • Easy storage and handling: Methanol does not need to be refrigerated like LNG, as it is liquid at ambient temperature and pressure. This simplifies storage and reduces costs for special tanks and equipment. Compared to hydrogen or LNG, methanol is easier to handle and requires less complex infrastructure.
  • Safety: Methanol is biodegradable and dissolves in water, which means there is less environmental damage in the event of an accident than with fossil fuels or ammonia, for example. Methanol is also less explosive than LNG or hydrogen. 
Youtube Video

Rolls-Royce engineers are already testing methanol combustion with a technology demonstrator on the test bench. They are working in parallel on concepts for single-fuel methanol engines that only burn methanol in the Otto process and on dual-fuel engines. These are compression-ignition engines that can run on both diesel and methanol. The single-fuel methanol engine is being developed as part of the publicly funded MeOHmare project. 

The first trials with complete mtu methanol engines on the test bench are scheduled for 2025.

The development of methanol engines is therefore a challenge

"In a few months' time, we will be testing the first mtu methanol engine on the test bench," explains Dr. Johannes Kech, who heads up the development of mtu methanol engines at Rolls-Royce. He can hardly wait for the moment when the first engine is running and the developers can see how the combustion process proves itself in a full engine and interacts with the specially developed turbocharging system. Together with his team, he has had to solve a number of challenges over the past few months. And he still has just as many ahead of him. 

"Developing a methanol engine is no trivial matter," explains Kech. He is particularly concerned with two issues when it comes to a pure single-fuel methanol engine: injection and mixture formation. "There are simply no injectors for methanol engines on the market for our power class that have a long enough service life," explains Kech.  

It is also complicated to have a homogeneous fuel-air mixture in the combustion chamber that can burn cleanly. This is because the lower lubricity of methanol means that the fuel cannot be shot into the combustion chamber at 2000 bar or more pressure like diesel. However, the lower the pressure, the more difficult it is to create a homogeneous mixture in the combustion chamber. "Put simply, the finest possible droplets of methanol must be present throughout the combustion chamber so that they evaporate quickly in order to ensure a homogeneous and ignitable mixture at the spark plug," says Kech.

But both Johannes Kech and Denise Kurtulus are convinced that the effort will be worth it. After all, green methanol can not only be used to power ships in a climate-neutral way. Burning methanol in the engine also produces far fewer nitrogen oxides and particles than running engines on diesel fuel. A complex exhaust gas aftertreatment system as with diesel engines will not be necessary. Any hydrocarbons produced by unburned or incompletely burned fuel can be converted using a catalytic converter. "In shipping, there is no way around methanol," says Kurtulus. 

Not trivial, but worth the effort: Injection and mixture formation are the biggest challenges in the development of methanol engines.

Methanol dual-fuel engines as a bridging technology

"In the long term, we see pure methanol single-fuel engines as the best solution," she says. At the same time, however, she recognizes the concern of many customers that green methanol will not be widely available in the medium term. For this reason, the Rolls-Royce engineers have also turned their attention to dual-fuel engines. "We see dual-fuel engines primarily as a bridging technology until green methanol is available across the board," says Kurtulus. "However, the length of this bridge varies depending on the application," says the expert. Yachts that call at ports all over the world will certainly rely on flexible dual-fuel propulsion for longer than ferry or tugboat operators who know their ports and therefore their fuel infrastructure. 

However, the development of a dual-fuel methanol engine is not easy either. Here, Kech and his colleagues are more in the comfort zone - after all, this is also about self-igniting engines in which diesel is injected into the combustion chamber.  But the aim here is to get by with as little diesel as possible. What's more, the existing diesel injectors now have to inject much smaller quantities of diesel. At the same time, the combustion chamber of the engine must not be optimized for methanol combustion, as the engine must continue to function in pure diesel mode. Compromises must therefore be made that limit the substitution rate and/or the efficiency of the engine.

There is no such thing as a "silver bullet"

However, both Denise Kurtulus and Johannes Kech are certain that the development effort is important. Both are convinced that there will not be just one single solution for environmentally friendly ship propulsion systems in the future. "There is no such 'silver bullet'," they emphasize. Instead, various solutions based on renewable energies are needed. One of these solutions will be mtu methanol engines. And they are not alone in this conviction. The Danish shipping company Maersk is already relying heavily on methanol. Not only has the company already put the first methanol-powered container ship into operation, it has also ordered over 20 more such ships. And as demand increases, so does the production of green methanol. 

Global production of e-methanol

The world's first commercial plant for the production of green e-methanol started production in Kassø in southern Denmark at the beginning of 2025. The aim is to produce 35,000 tons of e-methanol per year.  The green electricity for this comes from a neighboring 350-hectare solar park and a Danish wind farm. Meanwhile, the CO2 required for green methanol production is supplied by a biogas plant near Tønder. There, the raw biogas is separated into biomethane, which is fed into the gas grid, and CO2.

Anyang in China has been producing CO2 methanol on a commercial scale for over two years now. Up to 110,000 tons of liquid methanol per year are produced here from carbon dioxide, which is recovered from the existing emissions from lime production. The hydrogen is obtained from the gas from the coke ovens.

In Germany, more precisely in a chemical park in Leuna, green methanol has been produced in a pilot plant since November 2023. Although this plant is smaller than those in Denmark and China, the production process is considered to be particularly cost-efficient. It is based on a novel, three-dimensionally scalable, homogeneous catalysis that works more efficiently and under simpler conditions than conventional processes. 

"When the time comes, we will be ready"

"It will be a while before there is enough green methanol in the world to convert entire fleets of ships to methanol propulsion," says Kurtulus.  Experts assume that "But when the time comes, we will be ready," says the marine expert.   

STORY Commercial Marine

25 years of excellence: Series 8000

From the turn of the millennium to Today: The mtu 8000 Series has evolved from a groundbreaking innovation to the global standard for speed, efficiency, and reliability.

by Celina Dörge

Read more

STORY Yacht

Quartet of innovations: The new integrated mtu yacht systems

With an integrated bridge, an mtu powerhouse as its engine, and an efficient POD system, Rolls-Royce is setting new standards for performance, safety, and sustainability on board yachts.

by Rebecca Lorenz

Read more

STORY Commercial Marine

Leadership with attitude

Elegance and glamour on luxury yachts, dust in mines – Denise Kurtulus combines two worlds. As head of Rolls-Royce's global marine and mining business, she demonstrates that leadership is a question of attitude.

by Lucie Maluck

Read more

STORY Commercial Marine

Offshore boom in China: New ship for wind turbine maintenance

The offshore wind industry in China is booming. A new, very special ship is to help maintain wind turbines.

by Lucie Maluck

Read more

Connect with Us

Customer Assistance Center

We are here to take your Sales & Service questions around the clock, 365 days a year.

Read more

Sales & Service Locator

Find your local partner for Sales & Service.

Read more

mtu Stories

Reports and interviews about mtu products and solutions.

Read more