STORY Commercial Marine

Premiere in China: mtu engines power windpark service ships

Posted on May 18, 2021 by Julia Rieß, Images by Aurora (Dalian) Yachts Co.

Small, light, but impressive: mtu 8V2000M72 units have enabled Rolls-Royce to step into the Chinese offshore energy market, with very good prospects.

China's star is rising in the field of new energies, including offshore windparks. The first offshore windpark in China was built in 2009 and since then, the Chinese have been thinking big when it comes to expansion of wind energy in the country. By 2019, China ranked third in offshore wind energy with 5 GW output. According to figures from the Global Wind Energy Council (GWEC), that figure had now increased to 6.8 GW.  

So wind energy represents a gigantic future market in which it is worthwhile for Rolls-Royce to gain a foothold. That is because, as the number of windparks increases, so does the demand for wind park service vessels, which are absolutely essential for operation and maintenance of the huge turbine towers out at sea. These are vessels that require powerful and reliable propulsion systems to fulfil their mission.

Furthermore, since the new offshore wind parks are being built at ever greater distances from the coast, an even higher performance is needed from the vessels that serve them. And since they have a service life of some 20 to 25 years, they also need regular maintenance throughout that time to keep operation up and running. This is where the wind park service vessels come in, which bring the service engineers out to the parks, where they climb up to the turbine on a ladder. While the engineers make the transfer from ship to ladder, the vessel must stay in contact with the base of the turbine tower the whole time, however rough the sea conditions. That demands a very powerful drive. Furthermore, the bringing of personnel, spare parts, consumables and auxiliary supplies to the wind parks requires vessels that can be relied upon, however challenging the sea and weather conditions.  

The vessels were built by the shipyard Aurora (Dalian) Yachts Co. One 20m vessel can accommodate up to 12 engineers.

Rolls-Royce specializes in propulsion systems based on their compact, powerful, robust and reliable mtu marine engines that meet all these requirements. And since they boast the twin benefits of lower consumption and reduced emissions, mtu marine engines are not only highly cost-effective, but ecologically sound as well. These are the assets that Chinese shipyard Aurora shipyard was keen to gain as it opted to equip each of two new service ships with twin mtu 8V 2000 M72 units. These serve maintenance of a wind park run by State Power Investment Corp (SPIC), a large state-owned company and major player in the offshore wind energy market of Jiangsu province.

The vessels themselves – the Yifeng 02 and Dian Tou 02 – were built by the shipyard Aurora (Dalian) Yachts Co. under a license granted by Dutch  shipyard Damen Shipyards Group for construction of its vessel type FCS 2008 Twin Axe Fast Crew Supplier. The 20m vessel can accommodate up to 12 engineers. Each vessel has two small engine rooms in which one engine with peripherals fits. That is why not only high output, but small dimensions and light weight are required of the engine. mtu Series 2000 units, more than any other engines on the market, tick all these boxes. With a power output of 2 x 720 kW (around 1932 hp), the vessels reach speeds as high as 25 knots (46.3 km/h).

As Richard Wang, Marine Sales Director at mtu China, points out: “In terms of criteria such as dynamic performance, acceleration capabilities, low fuel consumption and others, these engines have the edge over our competitors.”

That puts Rolls-Royce in an excellent position to meet the challenges lying ahead on the Chinese energy market.  

Direct current, alternating current, emergency power

by Lucie Maluck

There is plenty of electricity in the huge offshore wind farms. Nevertheless, mtu emergency power aggregates are indispensable. Why?

Read more

Commercial Marine

Fast ship as an alternative to the helicopter.

by Lucie Maluck

High-speed crew transport vessel from Damen revolutionizes offshore crew change business model.

Read more

Commercial Marine

Safe transfer in the Elbe Estuary

by Dipl.-Ing Peter Pospiech

Trials success for new-concept pilot tender. The compact hull cylinder accommodates an mtu 10V 2000 M72 propulsion engine.

Read more

Connect with Us

Customer Assistance Center

We are here to take your Sales & Service questions around the clock, 365 days a year.

Read more

Sales & Service Locator

Find your local partner for Sales & Service.

Read more

mtu Stories

Reports and interviews about mtu products and solutions.

Read more