PRESS RELEASE Corporate

Backup power supply concept with renewable energy sources and mtu Onsite Energy CHP successfully tested

Posted on December 04, 2018

In November 2018, LEW Verteilnetz GmbH, mtu Onsite Energy and additional project partners from industry and science received the Bavarian Energy Award for the LINDA project.

Images [3 Files, 7 MB]

  • 185 photovoltaic systems, 2 hydroelectric power plants and a biogas plant form an autonomous power supply network for 3 local communities and 1,100 households
  • Gas-powered gensets prove ideal as leading power plants in the islanded grid

In November 2018, LEW Verteilnetz GmbH, mtu Onsite Energy and additional project partners from industry and science received the Bavarian Energy Award for the LINDA project. LINDA stands for local island power supply and accelerated grid restoration with distributed generation systems in the event of large-scale outages. In a number of field trials in an isolated network, a backup power supply concept based on renewable energy sources and mtu Onsite Energy CHP plants was successfully tested. The brand mtu Onsite Energy is part of Rolls-Royce Power Systems.

Securing the supply of backup power with renewables


The project background: a long-term, large-scale power outage can have serious consequences for nearly all areas of society like healthcare, IT, transport and traffic. Those involved in the project demonstrated that distributed generation units, such as photovoltaic systems, hydroelectric power plants and biogas plants, can be used to supply emergency backup power in the event of an outage. To this end, the project partners developed a concept and have now tested it successfully in what have been the most extensive field trials in an isolated grid in Germany to date: in three Bavarian communities, 1,100 households, 185 photovoltaic systems, two hydroelectric power plants and a biogas plant were interconnected in an autonomous islanded grid for a period of six hours. "In the course of carrying out the field trials, stable stand-alone mode operation was possible at all times," said Dr. Georg Kerber, project manager at LEW Verteilnetz GmbH.

The LINDA concept focuses primarily on the supply of emergency backup power for critical infrastructures, such as hospitals or drinking water supply systems. In the event of a power outage, they can be supplied with power from an islanded grid (microgrid) that is not connected to the national grid. Photovoltaic systems have not been used to provide a backup power supply to date, as these systems are dependent on an existing grid supplying a stable voltage and frequency. As a result of LINDA, such distributed generation units can now be made available to supply emergency backup power: a power plant with black start capability, in other words one that can start up on its own without the need for electric power, acts as the leading power plant and ensures that the frequency remains stable at 50 Hz. Due to the given power ratio this was performed by a hydroelectric power plant. The biogas plant based on mtu Onsite Energy gas generator sets was tested on its frequency stability. Photovoltaic systems thus recognise that a grid is in place and begin to supply the grid with electric power as if they were operating in a typical interconnected network. With the exception of modifications to the leading power plant, no retrofits to the systems are necessary. The concept can be applied quite well to other systems. LINDA is thus a key element in bringing about the energy transition and improving power supply reliability.

Gas-powered generator sets prove ideal as leading power plants in the islanded grid


In order to employ the backup power supply concept on a wide scale, the possibility of applying the concept to gas-powered generator sets as leading power plants in an islanded grid was also investigated on test benches using mtu engines. "Due to the widespread use of gas-fired power plants, their black start capability and their high availability levels, this type of power plant is extremely interesting for its use as a leading power plant," says Marcus Mücke, Head of Automation Systems Development at mtu Onsite Energy. "The results show that gas engines and biogas plants can be used as leading power plants." Rolls-Royce Power Systems will incorporate the new insights of this project into its further developed product portfolio of turnkey microgrids.

Project participants from industry and science


The project LINDA was developed and implemented under the leadership of LEW Verteilnetz GmbH, with partners from industry, such as MTU Onsite Energy GmbH, Bayerische Elektrizitätswerke GmbH, Stellba Hydro GmbH & Co KG, Marquis Automatisierungstechnik GmbH, PSI Software AG, and science, such as Augsburg University of Applied Sciences and the Technical University of Munich.
Silke Rockenstein Spokeswoman Trade Media
Phone:
+49 7541 90 7740
E-mail: