PRESS RELEASE Corporate

Quiet, clean and fast – mtu hybrid drive from Rolls-Royce for Lake Constance Belt Railway

Posted on May 08, 2018

The mtu Hybrid PowerPack from Rolls-Royce could be used on the Lake Constance Belt Railway (Bodenseegürtelbahn) and thus simultaneously provide environmentally friendly, economic and reliable rail operations even before electrification of the line.

Images [2 Files, 4 MB]

  • Successful simulation of hybrid train operation on Lake Constance Belt Railway
  • mtu Hybrid PowerPack reduces emissions, noise levels and operating costs on the existing infrastructure
  • Development is part of the Rolls-Royce electrification strategy

Friedrichshafen, Germany – The mtu Hybrid PowerPack from Rolls-Royce could be used on the Lake Constance Belt Railway (Bodenseegürtelbahn) and thus simultaneously provide environmentally friendly, economic and reliable rail operations even before electrification of the line. These are the findings of simulations that have been carried out by mtu on behalf of the Lake Constance Belt Railway community of interest (Interessenverband Bodenseegürtelbahn). Local emission-free operations, in urban areas and tunnels, for example, are feasible. Compared with a train driven by diesel engines alone, CO2 emissions can be reduced by up to 20 per cent using the hybrid drive system on this route. Generally speaking, these findings are also applicable to other routes. On an mtu test bench, the route between Radolfzell and Friedrichshafen was covered with a real-life Hybrid PowerPack and a computer-simulated environment (consisting of vehicle and route). It was shown that trains equipped with the mtu hybrid drive were able to keep to current timetables and timetables required in the future.

“With the Hybrid PowerPack, we are offering an environmentally-friendly rail drive solution that combines the benefits of battery and diesel-driven trains,“ said Lars Kräft, Vice President Industrial Business at Rolls-Royce Power Systems. “Trains fitted with our hybrid drive system could improve operations on the Lake Constance Belt Railway within just a few years – with considerably less noise, fewer emissions and more connections with more stops – and this can be done with no additional infrastructure costs.“

The operation of the current VT 612 railcar was simulated – it had been retrofitted in virtual reality with mtu Hybrid PowerPacks. That such a retrofit is also possible in a real-world environment has also been demonstrated by a feasibility study carried out by the Deutsche Bahn subsidiary, DB Systemtechnik. This is particularly relevant because these are vehicles that travel fast on curving track. Only these trains, which are fitted with “tilt technology“, are able to negotiate the numerous curves encountered on the Lake Constance Belt Railway track at high speed and thus provide a fast service between Basel and Ulm.

The mtu Hybrid PowerPack is a high-tech product from Friedrichshafen and the result of collaboration between the local companies Rolls-Royce Power Systems and ZF Friedrichshafen. It combines the following components to produce an intelligent drive system: a modern mtu diesel engine with exhaust gas aftertreatment, which meets current emission regulations in addition to the future EU Stage V that will come into force as of 2021, an innovative ZF automatic transmission, an electric motor that recovers energy in braking mode and also serves as a drive unit, and an advanced battery system to store the recovered brake energy. The Hybrid PowerPack has demonstrated its reliability, for example, in real-life test runs with a length of around 15,000 kilometres.

The technology is an important milestone on the way to the hybridisation and electrification of mtu drive systems, which are a current focus of developments at Rolls-Royce Power Systems. The company is working on a range of technologies now being developed primarily for rail, marine and power generation applications, which are to go into series production in the near future. These include so-called microgrid energy systems, which combine solar energy, gas gensets and battery storage systems. But hybrid drive systems for yachts will also be included in the range of products available from mtu in the future.
Silke Rockenstein Spokeswoman Trade Media
Phone:
+49 7541 90 7740
E-mail: