PRESS RELEASE Power Generation

Avacon uses mtu battery container from Rolls-Royce to test energy community concept of the future

Posted on February 23, 2021

Images [2 Files, 1 MB]

  • Field testing of how to integrate renewable energies into regional power grid
  • Aim is to provide sustainable, efficient, and reliable electrical power 
 

An mtu EnergyPack from Rolls-Royce is at the center of a field test begin carried out in the German State of Niedersachsen with the aim of supplying power sustainably and as far as possible independently of the public utility grid. The project name is ‘energy platform Twistringen’ and in it grid operator Avacon is simulating the operation of local grids by energy communities independently of the public grid. Part of the project involves the delivery by Rolls-Royce to Avacon Netz GmbH of a 20-ft mtu battery container with 1,000 kWh capacity and 800 kVA output. 

The growing demand for electrical power and the call for climate-neutral, efficient power generation represents a challenge to grid operators like Avacon. New solutions need to be developed and one of them could be the formation of local energy communities' who obtain their electrical power from wind turbines, solar panels and electrical generator sets.  In the current pilot project, Avacon is examining how such an energy community could generate, store and consume electrical power. The main job of the mtu EnergyPack will be to bridge the gap between the supply of green energy, which tends to fluctuate, and the power needs of households and businesses within the local grid. The project is being officially launched in a few weeks’ time, when voluntary participants in the region will join the local energy supply system and receive as much locally generated electrical power as possible by means of an intelligent control system combined with the mtu EnergyPack. 

“The mtu EnergyPack stores the electrical power generated from whatever source and makes it available to the energy community as and when required,” explained Cordelia Thielitz, head of the Microgrid Solutions division in the Rolls-Royce business unit Power Systems. “That makes it possible to cover a large part of the energy demand using electrical power generated from renewables, thereby saving on fossil fuels. In other words, batteries can be deployed in different energy landscapes and they also enable existing energy systems to be enhanced with up-to-date technologies.” 

The project is supported by PlatOne (PLATform for Operation of distribution Networks), a consortium of energy grid partners funded by the EU.  

About Rolls-Royce Holdings plc

  1. Rolls-Royce pioneers cutting-edge technologies that deliver clean, safe and competitive solutions to meet our planet’s vital power needs.
  2. Rolls-Royce Power Systems is headquartered in Friedrichshafen in southern Germany and employs around 10,000 people. The product portfolio includes mtu-brand high-speed engines and propulsion systems for ships, power generation, heavy land, rail and defence vehicles and for the oil and gas industry as well as diesel and gas systems and battery containers for mission critical, standby and continuous power, combined generation of heat and power, and microgrids.
  3. Rolls-Royce has customers in more than 150 countries, comprising more than 400 airlines and leasing customers, 160 armed forces, 70 navies, and more than 5,000 power and nuclear customers.
  4. Annual underlying revenue was £15.45 billion in 2019, around half of which came from the provision of aftermarket services.
  5. In 2019, Rolls-Royce invested £1.46 billion on research and development. We also support a global network of 29 University Technology Centres, which position Rolls-Royce engineers at the forefront of scientific research.

 

 

Contacts

Silke Rockenstein Spokeswoman Trade Media
Phone:
+49 7541 90 7740
E-mail: