Rolls-Royce Power Systems
PRESS RELEASE Naval Solutions

Rolls-Royce is strengthening digital training for the German Navy

Posted on June 10, 2026

Images [4 Files, 14 MB]

  • Real-world training for naval marine engineers at the Naval Engineering School in Parow
  • Virtual maintenance, diagnostics and troubleshooting on the mtu Series 4000 engine
  • A combination of a realistic training engine, augmented reality and virtual reality
  • Preparation for service on board the ‘Baden-Württemberg’ class F125 frigates long before the first rough seas

Rolls-Royce Power Systems is digitising the training of naval engineers at the German Navy’s Naval Engineering School (MTS) in Parow. Instead of practising in the engine room for the first time, trainees are now able to train on land using a realistic model of the 20-cylinder engine from the mtu 4000 series. Augmented reality and specially developed software realistically simulate maintenance, diagnostics and fault scenarios – long before the technicians board an F125 frigate. In this way, the company is supporting the German Armed Forces in the marine engineering training of future naval personnel.

“A stationary engine combined with 3D and augmented reality technology – that’s something the Bundeswehr hasn’t had before. For the first time, fault and damage scenarios can be simulated realistically. Participants practise not only diagnosis but also troubleshooting before they go on board. This ensures they are prepared when every minute counts. The fact that the Naval Technical School has placed its trust in us for this is of great significance to us,” said Knut Müller, Senior Vice President Global Governmental Business at Rolls-Royce Power Systems.

“What is new is that, for the F125, we are simulating real operational conditions on land for the first time: the same engine, the same engine management system and the same tools. The training is supplemented by augmented reality and 3D visualisations. This allows the ship’s engineers to experience maintenance and fault scenarios in a realistic manner before they go on board,” said the project coordinator responsible at the Federal Office for Equipment, Information Technology and Use of the Bundeswehr (BAAINBw).

Since March 2026, a 20-cylinder engine from the mtu 4000 series has been available for training at the Naval Engineering School. This is a so-called ‘cold model’ of the mtu 20V 4000 M53B engine. This is identical to the engine on board the German frigate F125 – but without operating fluids such as fuel, oil or compressed air. On board the ‘Baden-Württemberg’ class F125 are four mtu units, which are used for both on-board power and propulsion. Rolls-Royce Power Systems has designed these units specifically to meet the German Navy’s high standards. The mtu 20V 4000 M53B engine not only meets the particularly stringent shock requirements but also operates at a very low noise level.

The new training software gives marine engineers access to all relevant documentation: from diagnostic guides to maintenance and repair procedures. A functional engine management system enables the display of operating parameters as well as the simulation of realistic fault and damage scenarios. Augmented reality technology allows process-oriented troubleshooting activities to be clearly visualised. In addition, a virtual reality environment with a movable 3D model of the engine is available, in which assemblies can be visualised down to the level of small components.

Rolls-Royce Power Systems provides the full range of digital equipment for training: rugged Toughbooks, monitors, training computers and mobile devices. Practical work is not neglected either: for the engine, Rolls-Royce Power Systems supplies tools, assembly platforms and all the necessary components for realistic exercises.

About Rolls-Royce Holdings plc

  1. Rolls-Royce is a force for progress; powering, protecting and connecting people everywhere. Our products and service packages help our customers meet the growing need for power across multiple industries; enable governments to equip their armed forces with the power required to protect their citizens; and connect people, societies, cultures and economies together.
  2. Rolls-Royce has a local presence in 47 countries and customers in over a hundred more, including airlines and aircraft leasing companies, armed forces and navies, and marine and industrial customers.
  3. Through our multi-year transformation programme, we are building a high-performing, competitive, resilient and growing Rolls-Royce. We are building the financial capacity and agility to allow us to successfully develop and deliver the products that will support our customers through the energy transition.
  4. Annual underlying revenue was £20.1 billion in 2025, and underlying operating profit was £3.46 billion.
  5. Rolls-Royce Holdings plc is a publicly traded company (LSE: RR., ADR: RYCEY, LEI: 213800EC7997ZBLZJH69).
  6. Rolls-Royce Power Systems is headquartered in Friedrichshafen in southern Germany and employs more than 10,350 people. The product portfolio includes mtu-brand high-speed engines and propulsion systems for ships, heavy land, rail and defence vehicles and for the oil and gas industry. The portfolio also includes diesel and gas systems and battery containers for mission critical, standby and continuous power, combined generation of heat and power, and microgrids. With its climate friendly technologies, Rolls-Royce Power Systems is helping to drive the energy transition.

www.rolls-royce.com

Contact

Johannes Jerg Head of External Communications, Press Spokesman
Phone:
+49 7541 90 8979
E-mail: