PRESS RELEASE Power Generation

Tognum receives major order for gas turbine plant

Posted on September 11, 2008

The Tognum business unit Onsite Energy & Components is to supply an environmentally friendly gas turbine plant to Stora Enso Sachsen GmbH, a paper producer in Eilenburg, Germany. The investment volume amounts to approximately €10 million.
  • Order value of approximately €10 million
  • Gas turbine plant from mtu Onsite Energy to generate electricity and heat in Stora Enso paper factory

Friedrichshafen, 11. September 2008. The Tognum business unit Onsite Energy & Components is to supply an environmentally friendly gas turbine plant to Stora Enso Sachsen GmbH, a paper producer in Eilenburg, Germany. The investment volume amounts to approximately €10 million.

The plant to be supplied by mtu Onsite Energy works on the basis of the LM 2500 RD gas turbine. With a maximum electrical output of 34.5 megawatts and an electrical efficiency of better than 38%, it simultaneously generates electrical power and heat (cogeneration) from natural gas. This results in a total efficiency of 85%. Stora Enso will use the energy to process waste paper and produce recycled newsprint. The new cogeneration plant will replace the energy plant currently in use.

The compact design of the gas turbine plant from mtu Onsite Energy allows it to be installed in the existing power plant building without any difficulties. The entire installation of the plant, including start up and test operation, will be completed by the end of 2009 within a period of less than five months.

Fast installation was a key criterion for Stora Enso, because during the changeover phase, the company will have to purchase the energy required for the entire production facility externally at a significantly higher cost.

Stora Enso is one of the world’s leading paper producers and has operated the facility in Eilenburg in the German federal state of Saxony since 1994 for the production of newsprint, which is produced solely from waste paper.

- End -

Disclaimer regarding forward-looking statements et al.:


This report also contains forward-looking statements based on assumptions and estimates of Tognum’s Executive Board of Management. Although we assume that our assumptions and estimates on which we have based these forward-looking statements are realistic, we cannot guarantee that they will in the future prove to be correct. The assumptions and estimates, by their nature, may harbour risks and uncertainties that may cause the actual figures to differ considerably from the forward-looking statements. Factors that may cause such discrepancies include, among other things, changes in the economic and business envi¬ronment, variations in exchange and interest rates, the introduction of competing products, lack of acceptance for new products or services and changes in corporate strategy. Tognum does not undertake any obligation to update, to review or to confirm the forward-looking statements or to release publicly any revisions to any forward-looking statements to reflect events or circumstances after the date of this announcement.
Wolfgang Boller Spokesman Regional and Business Media
Phone:
+49 7541 90 2159
E-mail: