STORY

The mighty ones prefer mtu

Posted on February 14, 2018 by Lucie Maluck, Images by Oceanco

At the end of the day, luxury yachts are all about superlatives: on the deck and down in the engine room.

Number one is 180 m long, and in its engine room houses over 70 kW of drive power – it’s indisputably the most powerful mega-yacht in the world. Number two, the 138-m Rising Sun, is capable of delivering half of that output, so has no need to hide. Place no. 9 in the rankings is occupied by Indian Empress, 95-m long and boasting three 20-cylinder mtu units that deliver a whole 22,074 kW for acceleration up to 25 knots. At the end of the day, mega-yachts are all about superlatives: on the deck, luxury knows no limits, and down in the engine room, horsepower craziness reigns.  

The specialist journal “Boote Exklusiv” ('Exclusive Boats') has issued a ranking of the ten most powerful mega-yachts. Seven of them have mtu in their engine room. The propulsion concepts behind them are as varied as the yachts themselves. Some are straightforward and consist of mtu’s biggest and most powerful engine (the 20V 8000), that delivers 10,000 kW. In others, a combined solution with diesel engines and gas turbines has been chosen. These offer the advantage of fuel economy over long distances or during cruising, when just the diesel engine is brought on stream. When high speeds are needed, the gas turbine can be switched in.  These system packages include propulsion and automation, and are tailored by mtu to meet the customer’s specific needs. 

   

Point of contact

Anne Juhre
Phone:
+49 7541 90 2232
+49 7451 90 2232
+49 7541 90 7165
+79 7541 90 7165
E-mail:

Related stories

Commercial Marine Naval Solutions

mtu Virtual Marine Symposium provides impulses for the climate-friendly transformation of shipping

Read more

Yacht

Rolls-Royce and Sanlorenzo extend contract for mtu yacht propulsion systems

Read more

Yacht

Trade show highlights on the Mediterranean

by Katrin Auernhammer

In Cannes and Monaco, many yacht innovations will be lined up in September. It's all about design, size and propulsion. We feature some yachts with mtu engines.

Read more