STORY Power Generation

From potatoes to power

Posted on February 02, 2021 by Kerstin Hansmann, Images by Seydibey T.Ü.I.E.T.

Turkish foodstuffs producer Seydibey T.Ü.İ.E.T. processes around 70,000 metric tons of potatoes a year and sells them frozen in a wide variety of forms. A happy by-product of this is green electricity – produced with mtu gensets.
Konya, Turkey

Turkish foodstuffs producer Seydibey T.Ü.İ.E.T. has known for a long time that potatoes contain not just starch but also great potential. It processes around 70,000 metric tons of potatoes a year – and then sells them frozen in a wide variety of forms. A happy by-product of this is green electricity - produced with mtu gensets.

Whether it's french fries, croquettes, potato lattices or potato wedges – Seydibey products are popular with young and old. The company leads the market in this sector. All supermarket, restaurant and fast food chains in Turkey include the potato varieties in their assortments and menus. Seydibey T.Ü.İ.E.T. is a subsidiary of foodstuff conglomerate Konya Seker. Its production site is in the southwestern province of Konya, halfway between the cities of Seydişehir and Beysehir. So, it's no coincidence that its name is a cross between the names of the two cities. Since 2009, Seydibey has been processing potatoes there. 

 

“Large production volumes also create large amounts of waste, which at Seydibey consist mainly of potato peelings. As Turkey's largest producer of frozen potato products, we see it as our duty to recycle these sustainably"

Erman GÜMÜŞ, Director of Seydibey T.Ü.İ.E.T. plant.
The mtu CHP of the Series 12V4000L32FB converts the biogas into electricity and heat.

 

For this purpose, the company has set up a biogas plant on its production site, turning the organic waste into biogas. An mtu 12V4000L32FB combined heat-and-power plant (CHP plant) then converts the biogas into electricity and heat at a rate of 1,169 kW per hour. The process really pays off, with the ability to produce 9,000,000 kW of electricity per year which is then fed into the public power grid. The Turkish government rewards the production of green electricity, paying 0.133 dollars per kilowatt. An integrated heat recovery system ensures that waste heat from the biogas plant is made usable

For this project, the mtu CHP selected was the "tropical variant" of the 12V4000L32FB model.This refers to the special robust qualities of the engine used. It is deployed in places where the temperatures are particularly high. And a good thing too, because even though the Turkish province doesn't have a tropical climate, temperatures can quickly soar in the summer.  

Back in 2013, parent company Konya Seker installed a biogas plant with an mtu CHP plant on another production site, one run on a combination of biogas and fossil-based natural gas. Now the plant has been transported to Seydibey and put into operation there together with the new unit. Both plants are now biogas-only.

“We are proud to be operating our biogas plants using only environmentally friendly biogas. With the mtu CHP units, we have found a powerful and efficient solution for producing sustainable green electricity.”

Ali Arac, Technical Engineer at Seydibey T.Ü.İ.E.T.

And when the French Fries are sizzling in the pan, the power for them may be coming from the skins of the potatoes that are just becoming wedges and fries at Seydibey T.Ü.İ.E.T.

Energy Storage

When the wind falls silent and the sun goes to sleep

by Lucie Maluck

On the role of battery storage and gas-fired power plants in the energy transition.

Read more

Power Generation

How decentralized gas power plants are making energy supply more stable

by Lucie Maluck

What happens when the wind and sun take a break at the same time – and the grid reaches its limits? Rolls-Royce energy experts show how modular gas engine power plants keep the grid stable – flexibly, decentralized, and cost-efficiently.

Read more

Power Generation

AI boom: How combustion engines secure the power supply for data centers – and what Rolls-Royce is planning next

by Silke Rockenstein

Rolls-Royce has the most comprehensive portfolio for powering data centres – from diesel generators to SMR.

Read more