PRESS RELEASE Corporate

ROLLS-ROYCE POWER SYSTEMS INVESTS IN R&D FOR mtu ENGINES

Posted on July 27, 2015

Rolls-Royce Power Systems is investing in the development of next-generation combustion engines at mtu that stand out for their ecological soundness and cost efficiency.

Images [3 Files, 5 MB]

  • New R&D test facilities in Friedrichshafen already in service
  • 40 million euros for greater fuel economy and lower emissions

FRIEDRICHSHAFEN, GERMANY – Rolls-Royce Power Systems is investing in the development of next-generation combustion engines at mtu that stand out for their ecological soundness and cost efficiency. Today, the first new test stands in Friedrichshafen, mtu’s lead site and main R&D location, officially went into service. Rolls-Royce Power Systems has invested some 40 million euros in the new testing facilities at mtu. mtu is a Rolls-Royce Power Systems brand in the Rolls-Royce Land & Sea division.

"This move is making space for new developments in every sense of the word. Technology on the combustion engine of the future is going to be even more complex than that of its predecessors, so we have to make absolutely sure that we have the capacity to carry out tests and trials on our new products reliably and intensively," explained Dr Ulrich Dohle, CEO of Rolls-Royce Power Systems, at the opening ceremony. Rolls-Royce Power Systems will be using the new facilities not only to test further developments on existing engine series, but to break into new territories. New combustion processes, advanced technologies for electronic regulation and control and, from mid-2016, alternative fuels such as gas are some of the latest developments that will be put under scrutiny at the test stands.

A special feature of the new testing facility is the gallery that has been erected above each test stand booth. This will play a role in the development of exhaust aftertreatment systems: "Exhaust aftertreatment is one of our technologies for mtu engines. We are making a major research effort in this area because we want to develop diesel particulate filter and SCR technologies as far as we can ourselves. That will put us in a position to provide customers with a complete systems package." Exhaust aftertreatment systems will enable engines to meet the strict emissions standards coming into force in the future.

Today's ultra-modern test stands are the prerequisite for tomorrow's cutting-edge technologies. Chilling machines, heat exchangers, steam generators and various fuel formulations allow a whole spectrum of engine operation scenarios to be simulated - from biting cold to tropical humidity. State-of-the-art measuring and analysis systems support test stand technicians and development engineers in their work by enabling them to monitor results and   replicate and document them precisely.

Sophisticated technologies also come into play in the way the test stands themselves are run. In addition to conventional dynamometers, electrical gensets will also be used to simulate rapid load changes. The electrical power they deliver will also be fed into the factory's own power grid.

Construction of the 5-storey, 9,000 square-meter building that houses the test stands was begun in spring 2013 and recently completed. The first three test stands for testing 2,500-kW engines were set up in the first phase. Now underway is construction of a gas supply network for gas engine research that is to go into service in mid-2016. Further test stands can also be installed according to requirements.
Wolfgang Boller Spokesman Regional and Business Media
Phone:
+49 7541 90 2159
E-mail: