ROLLS-ROYCE WATERJETS AND mtu ENGINES SELECTED FOR NEW FAST FERRIES IN HONG KONG
Posted on March 02, 2018
Rolls-Royce has been contracted to deliver mtu engines and Kamewa waterjet propulsion units for three 42m high-speed, lightweight carbon fibre ferries for operation between Hong Kong and Guangzhou, China.
- Norwegian yard Brødrene Aa builds 3 high-speed ferries for Hong Kong
- Ferries are to be operated by Zhongshan-Hong Kong Passenger Shipping Co-op Co Ltd. between Hong Kong and Guangzhou
- mtu engines power more than 100 high-speed ferries in China
- Brødrene Aa opts for mtu engines and Kamewa waterjets also in Norwegian ferries
FRIEDRICHSHAFEN, GERMANY – Rolls-Royce has been contracted to deliver mtu engines and Kamewa waterjet propulsion units for three 42m high-speed, lightweight carbon fibre ferries for operation between Hong Kong and Guangzhou, China. The vessels will be built at the Brødrene Aa shipyard in Norway and are scheduled to be delivered to Hong Kong by June 2019.
This latest contract follows an existing order from the same shipyard for two similarly-sized ferries to serve routes in the north of Norway.
As well as Kamewa steel-series waterjets from Rolls-Royce, all five vessels will be powered by mtu series 2000 diesel engines. This combination offers the highest efficiency and lowest cost of ownership in the fast ferry propulsion market.
The Brødrene Aa yard has extensive experience in composite construction and launched its first carbon fibre ferry as long ago as 2002. Since then the yard’s designs and construction techniques have been continuously refined to meet the industry’s demands for more efficient ships, with lower emissions and reduced operating costs, saving weight without sacrificing safety or durability. The yard is today recognised as a world leader in fuel-efficient lightweight ferries. Currently they have started construction of their 60th carbon fibre vessel.
“With vessels operating long hours at speeds of 40 knots you really capitalise on the benefits of carbon fibre construction. Lighter vessels render lower fuel consumption and reduced emissions,” said Tor Øyvin Aa, CEO of Brødrene Aa. “The light weight and high-power capabilities of the Kamewa steel series waterjets, along with the proven power output and reliability of mtu engines in fast ferries, makes Rolls-Royce a logical choice for this type of vessel. However, the shipowners as always took the final decision about the main components, including the main engines and the waterjets.”
The Chinese ferries are to be operated by Zhongshan-Hong Kong Passenger Shipping Co-op Co Ltd. Two of the three vessels ordered will have a 300-passenger capacity and will operate at a maximum speed of 40 knots. They will have a quadruple Kamewa type S56-4 waterjet installation and four mtu 12V 2000M72 engines. The third will carry 230 passengers, with a maximum operating speed of 37 knots. This ship will be powered by two mtu engines 16V 2000M72, each driving a type S63-4 waterjet.
Knut Müller, Head of Marine and Governmental Business at mtu, said: “China is a very important market with great potential for us. In China and in the region around Hong Kong there are currently over one hundred high-speed ferries fitted with mtu propulsion systems in operation. We are delighted that with Brødrene Aa, with whom we have already collaborated on 25 other ferry projects, we have the opportunity once again of serving the Chinese market. High-speed ferries operate continuously at high speeds. For this reason, the engines must above all operate reliably over a long service life. mtu satisfies these demands placed on the engine with mtu's own turbocharger technology incorporating sequential turbocharging, which provides effortless power response at low engine speeds.”
The two Norwegian ferries have been ordered by the Nordland Fylkeskommune county municipality and will operate the Bødo-Sandnessjøen and Bødo-Svolvær coastal routes, jointly known as Nordlandekspressen. Nordland Fylkeskommune will own the ferries, and award a contract for the operation. The ferries will be delivered in December 2018 and February 2019.
The new ferries can carry 220 passengers plus 16 freight pallets weighing a total of 8 tonnes. The four mtu engines of the type 10V 2000M72 in each vessel will provide a service speed at 32 knots. Thanks to the efficient design of ship and propulsion plant, plus the light weight resulting from the carbon fibre reinforced sandwich construction, fuel consumption is anticipated to be around 30% lower than the existing ships.
mtu distributor Bertel O. Steen Teknikk has been supporting Brødrene Aa over many years both on application and on service side. In the Norwegian market, the distributor secures a strong position for mtu within the ferry market.
According to Tommi Viiperi, General Manager Sales at Rolls-Royce, these two contracts prove the high trust placed in Kamewa waterjets and mtu engines in both Norwegian and Chinese markets.
“The products selected and choice of materials and technologies are made for creating unchallenged performance, durability and the lowest cost of ownership. The efficiency of both steering and reversing units, together with pump performance, help owners to reduce their operational costs. The features included in our equipment are much appreciated in today’s market where there is no room for compromise on performance or efficiency. The duplex stainless steel construction of these Kamewa waterjets offers uncompromised durability compared with competing products. The fuel savings resulting from the highly efficient pump unit, combined with the design of the steering and reversing units, aids faster and more accurate manoeuvring,” said Viiperi.
Phone: |
+49 7541 90 7740
|
E-mail: |