STORY Power Generation

Walking the journey to Net Zero together

Posted on July 07, 2022 by Lucie Maluck, Images by Stefan Söll

At the mtu Power Generation Symposium, experts discussed how mtu solutions are helping to master the energy transition.

How can the global energy transition succeed? How can a realistic path to Net Zero be achieved? These were the leading questions of this year's PowerGen Symposium in Friedrichshafen. More than 300 customers and partners discussed this question with us, and actually everyone agreed: We need to walk the path to Net Zero together and start the journey today.    

Youtube Video

There is no question that energy is needed. The demand will increase massively in the coming years – especially for things like data centers that power our connected world. At the same time, security of supply is declining. The Ukraine war and the resulting gas crisis clearly show that both the availability and the quality of energy can no longer be taken for granted – and not just in Europe. The word needs power that can be produced reliably and climate-neutrally.  

Energy storage is the big challenge

One trend is already evident and will become even more pronounced in the future: The era of large power plants is ending; energy is increasingly being generated decentrally – and more sustainably, from renewable sources such as wind and sun. The challenge is that ideal conditions do not always exist for generating power through sustainable sources precisely when it is needed. Often the sun is not shining or the wind is not blowing.. Even then, energy must be made available. "The big challenge is to store the energy from renewable sources," said Tobias Ostermaier, President of Rolls-Royce's Stationary Power Solutions division. He presented the mtu EnergyPack for this purpose: Battery containers in the 550 to 2,200 kilowatt-hour capacity range. These store energy from renewable sources and make it available when it is needed.  

Electrolysers complete the mtu hydrogen ecosystem

Battery containers are not the only solution for energy storage. Electrolysers are another way to store energy by creating hydrogen. Beginning in 2024, Rolls-Royce will also provide these. Andreas Görtz, President of Rolls-Royce's Sustainable Power Solutions business unit, proudly announced the cooperation with Höller Electrolyzer. The company is currently developing a particularly efficient electrolyzer stack that will make electrolysis much more economical than before.  

The electrolyzers complete our product portfolio, and now we can offer products for the entire hydrogen ecosystem.

Andreas Görtz - President of the Business Unit Sustainable Solutions at Rolls-Royce Power Systems

This is because the electrolysers offer the second option for storing renewable energies - in the form of green hydrogen. This can be stored in tanks or pipelines and converted back into electricity as needed through mtu fuel cells or even hydrogen combustion engines.  

Youtube Video

Synthetic fuels and hydrogen blending enable rapid CO2 savings with existing products

It is not only with electrolysers and fuel cells that energy can be generated in a climate-neutral way. This is also possible with existing products that are already in use. For example, the CO2 emissions of diesel engines powered by HVO are reduced by up to 90 percent depending on the feedstock. The mtu Series 1600 and Series 4000 engines for the Power Generation sector have already been approved for use with HVO and other synthetic fuels complying with the EN15940 standard.   And the option of refueling the gas engines not exclusively with natural gas, but with a natural gas-hydrogen mixture, means that these engines can also be operated in a more environmentally friendly manner even today.   Soon, mtu gas engines will be able to run on a hydrogen content of 25 percent. This proportion is to be continuously increased until the engines can be operated with 100 percent hydrogen.


"We can provide each of our customers with the solution they need," Tobias Ostermaier summed up. Be it diesel or gas gensets, dynamic UPS, fuel cells, battery containers, electrolysers as well as interfaces connecting all these elements in a microgrid.’

STORY

Battery giants on the upswing: no energy transition without energy storage systems

How huge battery storage systems are becoming a key pillar of the energy transition.

by Lucie Maluck

Read more

STORY Power Generation

Greener power supply in the Seychelles

Seychelles aims to generate 15 per cent of its electricity from renewable sources by 2030. Three mtu EnergyPacks QL compensate for power fluctuations and thus stabilise the grid.

by Lucie Maluck, Kerstin Hansmann

Read more

STORY Power Generation

From food farmer to energy farmer

That's how a circular economy works: The Energor company collects food waste and uses it to make biogas that fuels twin mtu Combined Heat and Power modules. These generate enough electrical power for some 2000 households. We take a look behind the scenes at a very smart company.

by Lucie Maluck

Read more

Connect with Us

Customer Assistance Center

We are here to take your Sales & Service questions around the clock, 365 days a year.

Read more

Sales & Service Locator

Find your local partner for Sales & Service.

Read more

mtu Stories

Reports and interviews about mtu products and solutions.

Read more