Singapore’s data center industry, a cornerstone of its digital economy, faces dual pressures: meeting rising demand for reliable backup power while aligning with national net-zero 2050 targets and the Green DataCentre Roadmap (GDCR).
Internal combustion engines and generators remain a dependable and proven solution critical for grid resilience but may conflict with emissions-reduction goals of operators.
The GDCR’s objective of “using low-carbon energy to power the data center industry” is central and aligns with the use of Hydrotreated Vegetable Oil (HVO, Renewable Diesel) as a transitional solution with up to 90% CO2 savings while other solutions such e-Diesel (Power-to-Liquid = PtL) are being developed as low carbon long-term substitutes for fossil Diesel.
Examples of feedstock include crop-based feedstock such as palm oil which has been known to drive tropical deforestation, and waste-based feedstock, such as used cooking oil (UCO) and animal fats, which are more commonly used today. Further strategic policy interventions are essential to unlock sustainably sourced HVO and other longer-term low-carbon fuel solutions’ economic potential while advancing Singapore’s leadership in sustainable data center operations.
Microsoft and Rolls-Royce Power Systems are committed to reducing operational emissions and are focused on actively reducing CO2 emissions with HVO and other viable low-carbon fuel solutions that enable feedstock trace-ability along the value chain.
A collaborative approach between the data center industry, renewable fuel providers and policymakers is required to achieve a sustainable data center ecosystem. By leveraging existing infrastructure and offering targeted regulatory support, Singapore can help accelerate the transition to a low-carbon future for the data center industry. This will also advance climate objectives, stimulate economic growth, create jobs, and spur innovation.