Power Generation

Combined heat and power for residential & utilities

As the global population continues to grow, so does the demand for energy. The need for reliable, cost-effective energy chp solutions, especially for residential use, has never been greater.

Combined heat and power systems on and off grid

Energy quality and quality of life are closely interrelated. Particularly, residential power supply quality, reliability and rates play a key role. Combined heat and power (CHP) from gas gensets, possibly extended to a CHP microgrid solution with components such as battery energy storage systems (BESS), can enable substantial cost savings and increased sustainability.

mtu CHP and microgrid solutions do just that by ensuring the highly reliable and efficient supply of local power and heat, both on and off the grid, without the need for significant grid infrastructure investment or integration of renewable energy sources. Our diesel gensets excel at providing both prime and standby power.

mtu CHP plants for residential utilities

How to ensure CHP grid stability and make the most of renewable sources

Microgrids are ideal for areas where public grids are not available or cannot be upgraded quickly enough to meet growing power needs. mtu microgrid and other solutions maximize grid stability and clients’ green footprint through:

Voltage and frequency regulation
Smart battery energy storage systems (BESS) such as mtu EnergyPacks can greatly enhance residential power quality – for example, by providing grid services typically supplied by conventional power plants like voltage and frequency regulation.

Grid limitation management
The ability of BESS to reduce load peaks both during demand and generation also helps to defer the need for costly grid reinforcements – for example, in environments with limitations for the feed-in power of residential photovoltaic (PV) systems.
 

Arbitrage (energy trading)
The use of renewable energy sources enables BESS to optimize arbitrage (or energy trading) profits. They flexibly shift energy between tariff hours, storing it when prices are low and selling it when they are high.
 

Integration of renewable energy sources
Our microgrid solutions can be combined with a PV or wind power plant to enable quick compensation for short and medium-term fluctuations onsite. In essence, they turn variable renewable energy sources into reliable feeders.
 

Understanding off-grid energy supply

Download (PDF 120 KB)

Examples for off-grid energy supply

Download (PDF 1 MB)

Use case remote Vietnamese village

Download (PDF 657 KB)

CHP plants: How to use limited and valuable resources with optimal efficiency

Distributed energy supply solutions like our combined heat and power (CHP) systems are highly reliable and efficient, making them ideal for supplying residential complexes with power and heat. By using the waste heat with an absorption chiller, they even provide air conditioning. Powered by natural gas, they offer an extremely cost-effective, eco-friendly, compact and easy maintenance alternative to boiler-only plants.

How CHP systems ensure
power availability 24/7

In the event of a sudden power loss, mtu diesel gensets become real lifesavers, returning power to full load within a few seconds. Whether for prime or standby power, they deliver 24/7 for diverse power needs and transient loads – for large residential complexes and many other sensitive applications.

Need help finding the perfect CHP unit or system?

No problem at all. Let one of our CHP energy expert advisors point you in the right direction.

Power Generation

Coal island without coal: making the port of Duisburg CO₂-neutral

by Lucie Maluck

An intelligent, CO2-neutral energy system supplies a new terminal at Duisburg's inland port with self-sufficient green energy. At the heart of it all: two mtu combined heat and power units designed for operation with 100 percent hydrogen.

Read more

Power Generation

standby power generators: The back-up for the worst case scenario

by Vanessa Bösch, Anika Emmerich

mtu standby power generators are in demand like never before. What they can do, where to find them and what their climate-neutral future looks like.

Read more

Power Generation

When the wind falls silent and the sun goes to sleep

by Lucie Maluck

On the role of battery storage and gas-fired power plants in the energy transition.

Read more

Power Generation

Energy à la Brit: Gas Generators as Silent Winter Heroes

by Lucie Maluck, Anika Emmerich

Great Britain shows that it can be done without coal - almost! This winter, the proportion of coal in the electricity mix fell below one percent. Instead, the country is relying on wind and solar energy, nuclear power, biomass and mtu gas gensets.

Read more

Featured Case Study

Show all press content
Power Generation

Bringing power to Indonesia's communities: mtu delivers electricity to the most remote regions

20 February 2017

As Indonesia emerges as a leading developing economy, it faces a crucial challenge in its drive to bring a modern lifestyle to all of its citizens: supplying a consistent supply of power to its most isolated parts. To accomplish this, Indonesia’s state owned electricity provider – Perusahaan Listrik Negara (PLN) – turned to mtu.

Read More

Power Generation

Power Generation Solutions

Evolving Energy Landscape

Read more

Power Generation

Power Generation Products

More than just power.

Read more

Power Generation

Energy Storage System

The mtu EnergyPack battery storage system maximizes energy utilization, improving the reliability and profitability of your microgrid.