PRESS RELEASE Naval Solutions

Rolls-Royce to power Korea Coast Guard Patrol Boats with mtu engines

Posted on June 22, 2026

Images [2 Files, 11 MB]

  • Rolls-Royce will supply mtu engines for Korea Coast Guard’s new 50-ton and 500-ton patrol boat programs
  • The new boats will support fleet strengthening and enhance maritime security in the region

Rolls-Royce (LSE: RR., ADR: RYCEY) today announces it has been selected to supply mtu engines for two major Korea Coast Guard (KCG) patrol boat programs, supporting the strengthening of the fleet and expanding its maritime mission capabilities.

The KCG has announced the selection of mtu 16V 2000 M96 engines for its 50-ton class patrol boat program. Two shipsets, each equipped with two mtu 16V 2000 M96 engines, are scheduled for delivery by 2027. These new vessels will replace aging ships and enhance operational effectiveness. The overall plan calls for more than 50 shipsets over a 15-year period, ensuring sustained fleet renewal and long-term maritime security.

Additionally, mtu 20V 4000 M93L engines have been chosen for the KCG’s 500-ton class patrol boat program. Two shipsets, each with two mtu 20V 4000 M93L engines, are planned for delivery by 2027. These vessels are specifically designed to support the crackdown on illegal vessels, reinforcing the Coast Guard’s enforcement capabilities.

Michael Long, Vice President, Sales Governmental, APAC, Rolls-Royce Power Systems in Asia said:
“We are honored to support the Korea Coast Guard in its fleet strengthening efforts with our mtu Series 2000 and 4000 engines. These engines are engineered for reliability, efficiency, and performance, ensuring the Korea Coast Guard can respond swiftly and effectively to maritime challenges. Our ongoing partnership and technical support will help maximize operational uptime and mission success for the Korea Coast Guard.”

Both programs are currently in the design phase, with the first two ship construction orders scheduled for the second half of this year. 

About Rolls-Royce Holdings plc

  1. Rolls-Royce is a force for progress; powering, protecting and connecting people everywhere. Our products and service packages help our customers meet the growing need for power across multiple industries; enable governments to equip their armed forces with the power required to protect their citizens; and connect people, societies, cultures and economies together.
  2. Rolls-Royce has a local presence in 47 countries and customers in over a hundred more, including airlines and aircraft leasing companies, armed forces and navies, and marine and industrial customers.
  3. Through our multi-year transformation programme, we are building a high-performing, competitive, resilient and growing Rolls-Royce. We are building the financial capacity and agility to allow us to successfully develop and deliver the products that will support our customers through the energy transition.
  4. Annual underlying revenue was £20.1 billion in 2025, and underlying operating profit was £3.46 billion.
  5. Rolls-Royce Holdings plc is a publicly traded company (LSE: RR., ADR: RYCEY, LEI: 213800EC7997ZBLZJH69).
  6. Rolls-Royce Power Systems is headquartered in Friedrichshafen in southern Germany and employs more than 10,350 people. The product portfolio includes mtu-brand high-speed engines and propulsion systems for ships, heavy land, rail and defence vehicles and for the oil and gas industry. The portfolio also includes diesel and gas systems and battery containers for mission critical, standby and continuous power, combined generation of heat and power, and microgrids. With its climate friendly technologies, Rolls-Royce Power Systems is helping to drive the energy transition.

www.rolls-royce.com

Contact

Leng Wei Lin Regional Comms Lead - Asia
Phone:
+65 89073518
E-mail: