ProEXR File Description=Attributes=cameraAperture (float): 35.9999cameraFNumber (float): 8cameraFarClip (float): 1e+030cameraFarRange (float): 1e+018cameraFocalLength (float): 35cameraFov (float): 54.4322cameraNearClip (float): 0cameraNearRange (float): 0cameraProjection (int): 0cameraTargetDistance (float): 200cameraTransform (m44f): [{0.707107, -0.707107, -0, -3975}, {0, 0, -1, 191}, {0.707107, 0.707107, -0, -750}, {0, 0, 0, 1}]channels (chlist)compression (compression): ZipdataWindow (box2i): [0, 0, 14999, 9999]displayWindow (box2i): [0, 0, 14999, 9999]lineOrder (lineOrder): Increasing Yname (string): ""pixelAspectRatio (float): 1screenWindowCenter (v2f): [0, 0]screenWindowWidth (float): 1type (string): "scanlineimage"vrayInfo/camera (string): "RENDERCAM_Side35_shift"vrayInfo/computername (string): "desktop-a5as16d"vrayInfo/cpu (string): "INTEL/Model:15,Family:6,Stepping:2,Cache:0"vrayInfo/date (string): "2022/Jun/19"vrayInfo/filename (string): "//192.168.101.36/cgi01/ROLLS_ROYCE_SOLUTION/60679_023_Adaption_Rolls_Royce_Halle_2022/04_Rendering/scenes/RR_Halle_v009_IS.mb"vrayInfo/frame (string): "00001"vrayInfo/h (string): "10000"vrayInfo/mhz (string): "0MHz"vrayInfo/os (string): "Microsoft(tm) Windows(tm), version 6.2, "vrayInfo/primitives (string): "0"vrayInfo/ram (string): "130960MB"vrayInfo/renderlayer (string): "defaultRenderLayer"vrayInfo/rendertime (string): " 0h  0m  0.0s"vrayInfo/scenename (string): "RR_Halle_v009_IS"vrayInfo/time (string): "14:47:44"vrayInfo/vmem (string): "134217728MB"vrayInfo/vraycore (string): "3.60.04"vrayInfo/vrayversion (string): "Version of V-Ray for Maya 3.60.04"vrayInfo/w (string): "15000"=Channels=A (half)B (half)G (half)GI.B (half)GI.G (half)GI.R (half)Gesamtmaske.B (half)Gesamtmaske.G (half)Gesamtmaske.R (half)Multi_Matte_10_11_12.B (half)Multi_Matte_10_11_12.G (half)Multi_Matte_10_11_12.R (half)Multi_Matte_13_14_15.B (half)Multi_Matte_13_14_15.G (half)Multi_Matte_13_1
STORY Power Generation

Energy à la Brit: Gas Generators as Silent Winter Heroes

Posted on February 20, 2025, Images by Terra Firma Energy, Auchter Media

Great Britain shows that it can be done without coal - almost! This winter, the proportion of coal in the electricity mix fell below one percent. Instead, the country is relying on wind and solar energy, nuclear power, biomass and mtu gas gensets.
Droitwich Spa, UK
Find out more about mtu gas generator sets
Industries and locations may vary, but the need for constant power never changes.
Read more
They are as much a part of the UK as afternoon tea, Wimbledon or the Beatles: gas-fired power plants with mtu engines are indispensable for power generation in the UK. This is because the country - like so many others - relies on renewable energy sources to generate electricity. If these are not available, gensets with mtu gas engines step in.

What is special about the British model is that the operators of these gas gensets are not only paid when they provide electricity. They are also paid for their capacity to be available in times of need. “That makes it lucrative for the operators of gas-fired power plants, of course,” explains Ben Howkins, who manages sales of mtu engines for gensets in the UK.

500 mtu gensets support the British capacity market

Over 500 gensets powered by mtu gas engines are already in operation across the UK. Just recently, Terra Firma Energy in Droitwich Spa, UK, commissioned a new plant with two mtu-20V4000 L64 FNER gas gensets with a total output of 5 megawatts. They were supplied by Rolls-Royce's long-standing partner Yellow Power, which installs the mtu gas engines in containers. 

Two new mtu gas engines with a combined output of five megawatts have recently been commissioned in Droitwich Spa, UK.

“Normally, these generators are in operation for between 1,000 and 2,500 hours per year. Due to the unusually cold winter and the need for more grid capacity, the operating hours this year are likely to be higher,” said Howkins.

The mtu gas gensets are characterized by high efficiency and low emissions. As soon as green hydrogen is available and economical, they can also be converted to hydrogen engines and thus operated in a climate-neutral manner.

“The commissioning of our power plant in Droitwich is a testament to the power of partnerships and shared visions. Each of our partners has played a crucial role in making this project a reality, ensuring that it delivers flexible and reliable energy to meet the challenges of a modern electricity grid,” said William Davies, Managing Director of Terra Firma Energy at the opening of the plant.

Up to full load within 120 seconds

Gas genset power plants can be expanded within just twelve months as modular, containerized units and installed wherever there is access to the electricity grid and gas connections. The mtu gensets in Droitwich could be ramped up to full load within 120 seconds if required. As they are usually only operated at full power for a few hours two or three times a day, maintenance and overhaul costs are also low over the entire service life of the genset.

“With mtu's efficient, fast-starting gas gensets, the UK is securing its electricity supply - and taking an important step towards a renewable future,” said Howkins. An energy future that is set to be not only coal-free but also climate-neutral by 2035 - earlier than in the vast majority of European countries. 

Capacity market versus energy-only market

In an energy-only market, as is currently still the case in most European countries, only energy deliveries that actually take place are traded and remunerated. However, due to the growing share of renewable energies, the operating hours of conventional power plants are decreasing. This makes them less lucrative. However, the capacities of the power plants are still important. They are less in demand, but when they are, they have to be there. In a capacity market, however, it is not the electricity that is remunerated, but the provision of a certain capacity. The power plants therefore no longer sell electricity, but the security that electricity will always flow.

STORY Power Generation

How do gas engines differ from diesel engines?

Gas engines are experiencing a boom. A look under the hood reveals what sets them apart from diesel engines.

Read more

STORY Power Generation

When the Grid Can’t Keep Up: Powering the AI Era

The AI boom is driving global energy demand to unprecedented levels. Find out why grid capacity is increasingly becoming a bottleneck and how mtu solutions are helping pave the way for a digital future.

Read more

STORY Energy Storage

When the wind falls silent and the sun goes to sleep

On the role of battery storage and gas-fired power plants in the energy transition.

Read more

STORY Power Generation

How decentralized gas power plants are making energy supply more stable

What happens when the wind and sun take a break at the same time – and the grid reaches its limits? Rolls-Royce energy experts show how modular gas engine power plants keep the grid stable – flexibly, decentralized, and cost-efficiently.