PRESS RELEASE Power Generation

Rolls-Royce launches mtu hydrogen solutions for power generation

Posted on October 15, 2021

Images [1 Files, 1 MB]

  • From 2022 mtu Series 500 and Series 4000 ready for 25% hydrogen
  • From 2023 mtu engines and conversion kits available for 100% hydrogen

Rolls-Royce is further developing its mtu gas engine portfolio for power generation and cogeneration to run on hydrogen as a fuel and thus enable a climate-neutral energy supply. Already today, gensets powered by mtu Series 500 and Series 4000 gas engines can be operated with a gas blending of 10 percent hydrogen. Beginning in 2022, operation with a hydrogen content of 25 percent will be possible. “After intensive tests on test benches and pilot installations at customers in 2022, Rolls-Royce will continuously market new mtu Series 500 and Series 4000 gas engines beginning in 2023 for use with up to 100 percent hydrogen, and on a design to order basis  
conversion kits to allow already installed gas engines in the field to run on 100% hydrogen,” said Perry Kuiper, President Sustainable Power Solutions at Rolls-Royce Power Systems.

Power plants with hydrogen engines support energy transition
“The decarbonisation of power generation requires reliable, flexible, but also climate-neutral, power plants to supplement the fluctuating generation from wind and sun. We assume that natural gas will initially be the primary fuel in the development of the hydrogen ecosystem, but we see hydrogen as technically and economically possible. That is why we continue to develop our gas engines for use with green hydrogen - whether as a 10 or 25 percent admixture or for 100 percent," explains Andreas Görtz, Vice President Power Generation at Rolls-Royce Power Systems.

Rolls-Royce builds expertise for H2 ecosystem
In addition, fuel cells powered by 100% green hydrogen can play an important role in future energy supply in combination with renewable energies. At its Friedrichshafen headquarters, Rolls-Royce's Power Systems division has installed a 250-kilowatt fuel cell demonstrator, which will be used to test and present future CO2-free energy systems to customers. The entire hydrogen ecosystem, including the infrastructure for supply, conversion, test benches and future production, is also being mapped in the company's own plants, thus building up expertise.

Rolls-Royce focuses its climate protection programme Net Zero at Power Systems
on new technologies and fuels

With its climate protection programme "Net Zero at Power Systems", Rolls-Royce's Power Systems division has set itself the target of saving 35 per cent of greenhouse gas emissions by 2030 compared to 2019 using new technologies. This near-term target plays an important role in the Rolls-Royce Group's ambition to achieve carbon neutrality by 2050 at the latest. In addition to new technologies, a key element in achieving these targets is the certification of key mtu engine products to run on sustainable EN 15940 fuels such as e-diesel and second-generation biofuels as early as 2023.

  

About Rolls-Royce Holdings plc

  1. Rolls-Royce pioneers the power that matters to connect, power and protect society. We have pledged to achieve net zero greenhouse gas emissions in our operations by 2030. We joined the UN Race to Zero campaign in 2020, and have committed to ensuring our new products will be compatible with net zero operation by 2030, and all products will be compatible with net zero by 2050.
  2. Rolls-Royce Power Systems is headquartered in Friedrichshafen in southern Germany and employs around 9,000 people. The product portfolio includes mtu-brand high-speed engines and propulsion systems for ships, power generation, heavy land, rail and defence vehicles and for the oil and gas industry as well as diesel and gas systems and battery containers for mission critical, standby and continuous power, combined generation of heat and power, and microgrids.
  3. Rolls-Royce has customers in more than 150 countries, comprising more than 400 airlines and leasing customers, 160 armed forces and navies, and more than 5,000 power and nuclear customers.
  4. Annual underlying revenue was £11.76 billion in 2020 and we invested £1.25 billion on research and development. We also support a global network of 28 University Technology Centres, which position Rolls-Royce engineers at the forefront of scientific research.
  5. Rolls-Royce Holdings plc is a publicly traded company (LSE:RR., ADR: RYCEY, LEI: 213800EC7997ZBLZJH69).

Contacts

Silke Rockenstein Spokeswoman Trade Media
Phone:
+49 7541 90 7740
E-mail: