STORY

Automatically connected

Posted on January 25, 2017 by Lucie Maluck, Images by Robert Hack

To ensure a first-rate vehicle interface for a first-rate engine, mtu develops specific automation systems for each application.
Friedrichshafen, Germany

What use is a top-class engine if its vehicle connection is second-rate? It will certainly fail to make the most of its capabilities. Only when all the engine’s components are working in perfect harmony and are perfectly matched to the vehicle can it deliver its full potential. To ensure a first-rate vehicle interface for a first-rate engine, mtu develops specific automation systems for each application that manage, monitor and control the entire working of the drive system and other components, where the customer so requires.

A machine picks and places components on the PCBs. Employees in the electronics department place the strips with electronic components into this device – also known as a feeder.

An air-conditioned room, employees in white coats, and a quiet humming sound. Is that the image of an engine production bay? Sounds more like a dental surgery. Yet this large, sterile room is the manufacturing facility at the mtu Electronics Center. Low clicking and clunking noises are coming from a large white robot. A pick-and-place machine puts miniature components weighing just 5 mg, such as capacitors, resistors and diodes, onto a printed circuit board with millimeter precision. Depending on the electronic assembly in question, between 1,500 and 2,000 parts are placed via large rolls onto the PCB, where they are soldered into place. Connections are made.

They are connections without which the vehicles would not be able to move
independently, yet which are invisible to the train driver, haul truck driver or ship’s
captain. And they’re not the only ones. The locomotive builder, haul truck maker and shipbuilder also benefit from the many thousands of connections which mtu supplies between engine and vehicle or vessel. “Without wishing to sound arrogant, no other manufacturer makes it as easy for vehicle manufacturers to install their engines into vehicles and vessels,” said Martin Gohlke, who runs Automation Systems Development at mtu. “We are not just an engine maker, we’re a manufacturer of entire drive and propulsion systems,” he added. And these systems consist of an engine and the associated automation system.

One simple movement – complex connections


Here’s an example: A train driver wishes his train to accelerate. In the cab, he uses
the control lever on the driver’s console to send a signal via the vehicle control system and the mtu interface to the mtu automation system, which receives the message, processes it and forwards it to the engine governor, which in turn passes it to the engine. That’s quite a few connections already, but there are more. Within the engine, a further complex process is set in motion: Higher speed means that more fuel and more air have to arrive in the cylinder simultaneously. At the same time, the fuel pressure has to rise to ensure the fuel atomizes better.
Powerline integrates all monitoring, management and control functions of the diesel propulsion system.

As modern mtu engines always add a certain amount of exhaust gas to the fuel/air mixture as a means of minimizing nitrogen oxide emissions, the processor also takes data from sensors in the charge-air duct to calculate how much exhaust gas is required in the combustion chamber. It then forwards this data to the actuators via a ‘data bus’. The actuators convert these electronic signals into mechanical movements. In this instance, they move the air and gas valves and prolong the length of time the injectors are energized. A multitude of connections to which the train driver is probably oblivious when pushing the lever.

An engine is made up of hundreds of different parts and technologies. Every one is important, but the real trick is getting all the components to work together. No coincidence, therefore, that the engine management system and Engine Control Unit (governor) are known as the engine’s ‘brain’ connecting all those technologies together.

mtu automation: connecting the engine to the vehicle or vessel


However, the connections do not stop at the engine: the way it communicates with the vehicle or vessel is equally important. To ensure this runs perfectly, mtu develops the right automation system for each application – whether it be for locomotives, ships, haul trucks or electrical gensets. The Powerline automation system is available for locomotives, and for ships, Blue Vision NG and Callosum. Motivline has been designed specifically for haul trucks, and Genoline for gensets.

The Blue Vision New Generation automation system controls and monitors the entire propulsion system on board ships.

All the systems connect data from the engine management system to data from the vehicle control system and peripheral components such as radiators, transmissions and propellers. By so doing, they enable the manufacturer to install the engine into its vehicle or vessel with speed and ease. To help with this, mtu supplies pre-manufactured components developed in-house, which merely have to be hooked up to the vehicle control system. “The vehicle or vessel manufacturer only has to specify the scope of the automation system, tell us how long the cables should be, and then plug the drive system connector (supplied) into the vehicle control interface,” said Michael Welte, Manager System Engineering at mtu. And once the engine is running, the operator is fed all the information needed to make the very best use of the engine(s) and drive system in its installation. A perfect connection.

The automation systems are all designed along similar lines, consisting of a central Engine Control Unit which collates and processes the engine data which is then connected to the vehicle control system via standardized interfaces like CANopen, Ethernet and J1939. Another element is the Diagnostics and Remote System (DRS) via which mtu engineers program data and operating parameters such as engine speed bands, alarm limits or fan operating curves to the ECU. Later, operators can also use this DRS interface to obtain system and installation data from the engine or
propulsion plant via remote link.

A well-designed connection in two respects: the automation system
connects engine and vehicle as well as man and machine.

Simpler locomotive connection thanks to Powerline

Locomotive builders can use the standardized interfaces of the mtu ‘Powerline’ automation system to speed up the process of installing mtu engines in their trains.A CANopen bus interface standardized for data transfer ensures a fast connection between the engine and the locomotive’s central control system. External engine peripherals such as the cooling system, fuel treatment system or limit monitoring systems are also connected to the engine via the mtu automation system. At the heart of the system is the Power Automation Unit (PAU), the central interface between the engine and the locomotive control system. This connects the various locomotive control units easily to the mtu diesel engine. Signals typically exchanged between the locomotive control system and the PAU include things like engine start-up, engine shut-down and required engine speed. Important information such as current engine speed, oil pressure and coolant temperature are also processed by the PAU and displayed to the train driver via the instrumentation on the driver’s console. This all goes to make the PAU the driver’s central link to the engine and the central tool helping the train manufacturer build the Powerline drive system into the locomotive quickly and easily. Valid certification of the Powerline system creates yet another connection, namely to the technical assessor acting for the German Federal Rail Authority who approves implementation of the mtu system in the locomotive.

Connections on board ships: Blue Vision New Generation

In addition to other marine propulsion systems, mtu has developed the Blue Vision New Generation ship automation system to keep the communication going between a ship’s captain and the vessel’s engine. Different configuration levels are available: the simple, non-classifiable version ‘Blue Vision Basic New Generation’ and the enhanced classifiable version ‘Blue Vision Advanced New Generation’. A top-of-theline version ‘Blue Vision Basic New Generation’ is to be introduced at a later date. The automation system can be connected to the existing on-board ship’s system using standard interfaces such as J1939, CANopen or Ethernet. The heart of the system is the Local Operating Panel (LOP). As with the PAU in the Powerline rail system, the job of this LOP is to monitor and control the entire propulsion system. One example is when the ship is moving off: the captain moves the propulsion control lever to ‘50%’, giving the signal to move off. This information arrives at the LOP which then sends it to the transmission system, telling it to engage gear. Once this has happened, it tells the Engine Control Unit to increase engine speed. The LOP then tells the instrumentation on the bridge at how many revolutions per minute the ship’s engine is turning, how fast it is moving or how high the engine temperature is. “Our automation system could even track the temperature of a luxury yacht’s whirlpool and ensure the skipper is informed,” said Michael Welte.

Gensets - Genoline

For marine gensets (engines coupled to electric generators) which are used to generate power for diesel-electric propulsion or to supply on-board equipment, mtu has developed the Genoline automation system. Genoline monitors and controls the diesel engine and monitors the generator it is coupled up to. Here too, the heart of the system is the Local Operating Panel (LOP) which can be connected to the operator’s external system by means of a standardized J1939 or CANopen interface. The modular system makes it possible to fine-tune the diesel engine to the many different operating conditions that prevail when electricity is being generated. For example, when the winding temperature inside the generator rises too high, the genset is shut down automatically to protect the generator. A corresponding message is then produced which can be filtered out of the LOP display and conveyed to the external system interface. Project Genoline NG is currently underway to develop a new generation of automation specifically for these applications. Here, among other things, the system is being adapted in line with the latest mtu ‘MCS6’ automation technology, for example communicating via an Ethernet interface instead of CAN, and including both the possibility of adding a specific variant to meet the high standards required by military orders and enhanced compatibility with other engine series.


Point of contact

Martin Gohlke
Phone:
+49 7541 90 6200
+49(0)7541 906200
Fax:
+49(0)7541 90906200
E-mail:

Related stories

mtu NautIQ Master Advanced

mtu NautIQ Master Advanced provides a reliable and cost-effective Alarm and Monitoring System (AMS) solution for a wide range of vessel applications. Based on pre-engineered modules with built-in expansion capabilities, the system combines proven functionality with the flexibility to accommodate evolving operational requirements throughout the vessel's lifecycle. A selection of display systems supports different operating environments and console configurations.

Read more

mtu NautIQ Master Unlimited

mtu NautIQ Master Unlimited is an Integrated Platform Management System (IPMS) designed for naval, governmental and highly complex commercial vessel applications. Its scalable architecture supports the integration and management of critical onboard systems through a common operating environment.

Read more

mtu NautIQ Master Essential

Read more