CASE STUDY Power Generation

Suez Canal Corridor Relies on dynamic UPS

Posted on November 12, 2020

Uninterruptable power for 5.8 km tunnel facing environmental challenges with temperatures up to 40°C, and large amounts of sand.

Situation

The Suez Canal Corridor Development Project in Egypt aims at more effectively capitalizing on the Suez Canal, creating an integrated industrial and logistics zone to boost the country's economic growth. A rapid and easy link between both banks of the canal was essential in this project. Thus, the developers have planned the construction of high capacity road and rail tunnels at three locations: Port Said (North), Suez (South), and Ismailia (halfway between the two others).

With a total length of 5.8 km, its deepest point reaching 53 m under sea level, an internal diameter of 11.4m, and two lanes in each direction, the Ismailia twin-tube road tunnel is undoubtedly the most impressive part of the development. Especially considering the environmental challenges faced, as temperatures rise to up to 40°C, and large amounts of sand have to be dealt with.

Solution

To be operated safely, an infrastructure project of this nature requires a truckload of electro-mechanical equipment: lighting, road signage, ventilation, communication, fire detection, firefighting pump systems, smoke extraction, and a centralized control center. All of them must be fully operational in all circumstances, even in the case of a mains failure.

That is the reason why the client chose to equip the tunnel with 4 dynamic no-break systems, made by former Kinolt S.A. (Liège, Belgium) which Rolls-Royce acquired in 2020. The systems are now part of Rolls-Royce’s mtu portfolio and named mtu Kinetic PowerPack. Apart from the impressive constant heat-resistance of the units, the air inlets of the machine rooms are provided with performant sand traps and dust filters to deal with the vast amounts of sand at the site.

Result

In this specific case, traditional techniques did not allow sufficiently fast communication between both power plants, because of the approximately five kilometers of distance between them. Therefore, we developed a specific communication method for the cases where the two power plants need to communicate and share loads. At each end of the tunnel, we installed two units of 2000 kVA operating in parallel, in a dedicated technical building. Each set of two systems protects one tube. Due to the cable length, the energy is conveyed in the tunnel in 22 kV up to the points of use where local step-down transformers are installed.

Looking for Dynamic UPS related sales or service partners?

Power Generation

Sustainable Hybrid System ensures cost-effective power supply in Australia’s Northern Territory

Many aboriginal communities in the Northern Territory of Australia power their homes by electricity generated from diesel power plants. With the aim of reducing the dependence on diesel fuel and acquire the advantages of using renewable energy, Power and Water Corporation started a project located in small community of Daly River. The project expanded the power plant by implementing solar modules and a battery storage unit from the Rolls-Royce solution brand, mtu (former Qinous). The hybrid system project achieved a reliable 24/7 energy operation and currently reduces fuel consumption by 50 percent.

Read more

Power Generation

How we protect the environment and DNA samples from around the world

mtu Kinetic PowerPack for world's leading institutes and organizations in genomics and computational biology ensuring uninterruptable power to overcome some of humanity's most significant challenges.

Read more

Power Generation

E-vehicle superchargers in Austria more reliable thanks to mtu battery systems

Pull over, fill up, drive on – without losing time. What drivers of petrol-powered automobiles have long taken for granted will, over time, become the new norm for E-drivers too. Many utility grids tend to reach overload when having to cope with several E-vehicles being charged at the same time, or with super-chargers that are demanding high power delivery quickly. Now SYNERG-E, an EU-funded tech project, is helping E-vehicle service stations overcome these challenges at several locations in Austria. How? With stationary battery storage systems carrying the Rolls-Royce brand mtu.