However, the higher the proportion of wind and solar energy in the grid, the greater the importance of a word that was only added to the Duden dictionary in 2016: dark doldrums. It refers to times when the wind and sun do not provide any energy because it is either dark or there is no wind because it is calm.‘
Solar and wind power are volatile, and the peaks in power generation do not always coincide with the peaks in demand. To balance out these fluctuations and to be able to use the electricity generated at all times, more energy storage is urgently needed. For longer periods of dark doldrums, additional capacity reserves are needed,’ said Andreas Görtz, who heads the sustainable solutions business at Rolls-Royce's Power Systems division.
Two technologies will play a crucial role here: battery storage and gas-fired power plants.
mtu EnergyPacks: Storing green energy
On sunny or windy days, when the sun and wind generate more energy than is actually needed, battery systems such as the mtu EnergyPack QG store the surplus energy. This stored energy can be fed back into the grid later. In the event of sudden demand peaks or unexpected outages, battery storage systems can also react quickly and provide additional power at short notice.
But battery storage systems have even more advantages: they can supply or absorb energy in fractions of a second to compensate for fluctuations in the grid frequency. This is crucial to ensuring the stability of the power grid. By flexibly feeding energy into the grid, they help to smooth out peaks and reduce the load on grid components.
mtu battery energy storage system: modular units, flexibly scalable
With the mtu EnergyPack QG, Rolls-Royce supplies large-scale storage solutions consisting of modular units for capacity and power that can be flexibly configured. A large-scale mtu battery storage facility with an output of 291 megawatts and a storage capacity of 582 megawatt hours is currently being built in Lithuania. The battery systems store surplus electricity from renewable energies and feed it back into the power grid when demand increases, balancing the system and ensuring a reliable power supply.