Power Generation

mtu Kinetic PowerPack supports critical BBC services

Posted on 28 October 2020

Dynamic UPS for welsh headquarters of U.K.’s famous broadcasting station considering challenging noise level and space requirements.

Situation

The construction of the new headquarters of BBC Wales, in the summer of 2017, was one of the most significant developments undertaken in the country. Not only home to 1200 BBC staff, but also some of the most advanced broadcasting technologies and equipment, it is needless to say uninterrupted power is critical at the facility.

A well-considered selection process followed. Apart from uninterrupted power, efficient use of space was vital in the BBC's decision. The reason for the importance of this efficiency was, unlike its solution, slightly straight forward, to meet planning regulations, the BBC needed a sufficient amount of parking space in the building's basement.

Solution

Hence why today's mtu Kinetic PowerPack (formerly known as Kinolt KS) was selected as an answer to BBC's questions. The reason for this is the class-leading power density of the product, which is all thanks to its battery-free, compact design. Another primary concern for the BBC were noise levels. The nearby recording studios had to be isolated from any building plant noise.

According to the engineer manager, who was responsible for the project, the process was rather intense: “lt took place over several months and included technical evaluation of static UPS technology versus dynamic UPS. Eventually, we were able to develop a tailored UPS solution offering BBC not only trusted power but also giving them the maximum parking space in the basement, within project scope, and in line with budget limitations!”

Result

Teamwork was a large part of the process, he states; "Working with our acoustics partners, we delivered on the brief of achieving a 57 dBA noise level when the diesel engines operate. The installation consisted of two medium voltage 2750 kVA systems supporting a redundant A and B distribution network. BBC continues to enjoy our support as we have a 24/7/365 service support contract in place, including a four hour guaranteed response time."

"The requirements regarding noise and space posed a unique engineering challenge, and we  delivered a solution tailored to these specific needs. Once again, we demonstrated that we look at UPS from a client perspective."

Looking for Dynamic UPS related sales or service partners?

Power Generation

Sustainable Hybrid System ensures cost-effective power supply in Australia’s Northern Territory

Many aboriginal communities in the Northern Territory of Australia power their homes by electricity generated from diesel power plants. With the aim of reducing the dependence on diesel fuel and acquire the advantages of using renewable energy, Power and Water Corporation started a project located in small community of Daly River. The project expanded the power plant by implementing solar modules and a battery storage unit from the Rolls-Royce solution brand, mtu (former Qinous). The hybrid system project achieved a reliable 24/7 energy operation and currently reduces fuel consumption by 50 percent.

Read more

Power Generation

How we protect the environment and DNA samples from around the world

mtu Kinetic PowerPack for world's leading institutes and organizations in genomics and computational biology ensuring uninterruptable power to overcome some of humanity's most significant challenges.

Read more

Power Generation

Suez Canal Corridor Relies on dynamic UPS

Uninterruptable power for 5.8 km tunnel facing environmental challenges with temperatures up to 40°C, and large amounts of sand.