Rolls-Royce and Daimler Truck AG plan cooperation on stationary fuel-cell systems
Posted on May 26, 2020
- The Rolls-Royce Power Systems business unit focuses on development and sale of fuel-cell generators as mtu emergency power generators
- Fuel cells are to be supplied by the planned Daimler Truck AG and Volvo Group joint venture
- First demonstrator to be operational by end of year
Rolls-Royce plc and Daimler Truck AG plan to cooperate on stationary fuel-cell generators as CO2-neutral emergency power generators for safety-critical facilities such as data centers. They are to offer emission-free alternatives to diesel engines, which are currently used as emergency power generators or to cover peak loads. Daimler Truck AG and the British technology group Rolls-Royce have signed an agreement to this effect. A comprehensive cooperation agreement is to be prepared and signed by the end of the year.
Daimler and Rolls-Royce are linked not only by longstanding cooperation on conventional drive systems for other applications. At the end of last year, Rolls-Royce Power Systems and Lab1886, Daimler’s innovation unit for new business models, had already agreed on a pilot project to develop a demonstrator for the use of this technology for stationary power supply on the basis of fuel-cell modules from the automotive sector. It will go into operation in Friedrichshafen by the end of this year.
In April, Daimler Truck AG and the Volvo Group signed a preliminary, non-binding agreement to establish a new joint venture for the large-scale development, production and commercialization of fuel-cell systems for heavy-duty commercial vehicles and other applications. The Rolls-Royce Power Systems business unit plans to rely on these fuel-cell systems from the planned joint venture – as well as Daimler’s many years of experience – in the emergency power generators it develops and distributes for data centers under the mtu product and solution brand.
“Data centers are the nodes of the global information and communication network, whose vital importance has become particularly clear in these difficult times and whose operation must therefore be reliably safeguarded. The same applies to other safety-critical systems. Under our mtu brand, we develop customized solutions, thousands of which we have already installed, for data centers’ individual, complex and growing energy needs. The decarbonization of drive systems and power supply is one of our central strategic goals of our PS2030 strategy and fuel cells will play a key role in this. No other technology offers such high reliability, modular scalability and all the advantages of renewable energies without dependence on the conventional energy market. Through the cooperation with Daimler Trucks, we will gain access to fuel-cell systems that meet our demanding requirements and will thus further strengthen our outstanding position in this growth market,” said Andreas Schell, CEO of Rolls-Royce Power Systems.
“For Daimler Truck AG, fuel-cell systems play a decisive role in achieving CO2-neutral transport – as a supplement to battery-electric drive. Only End of April, we announced our intention to establish a joint venture with the Volvo Group. With the agreement for stationary fuel-cell systems concluded, we are already demonstrating very concrete opportunities for the commercialization of this technology through the joint venture,” stated Martin Daum, Chairman of the Board of Management of Daimler Truck AG and Member of the Board of Management of Daimler AG.
“We are delighted that Rolls-Royce is as convinced as we are of the future of fuel cells in the stationary sector and would like to enter into this long-term cooperation with us. On the one hand, this represents further impetus for the development of a hydrogen infrastructure across all sectors and applications; on the other hand, it will enable us to work together to further increase the economy of fuel cells, as well as society’s acceptance of and confidence in them,” continued Martin Daum.
Earlier large-scale production of fuel cells for stationary applications possible
Daimler Truck AG and the Volvo Group plan to start large-scale production of heavy-duty fuel-cell commercial vehicles for demanding and heavy long-haul applications in the second half of the decade. However, the fuel-cell systems for stationary applications can be produced in series by the planned joint venture between Daimler Truck AG and the Volvo Group at an earlier stage, as the specific requirements for use in transport on public roads do not apply.
During the past two decades, Daimler has already developed considerable expertise in fuel-cell technology with its site in Nabern, Germany (currently the headquarters of Mercedes-Benz Fuel Cell GmbH) and other production facilities in Germany and Canada. In order to enable the joint venture with the Volvo Group, Daimler Trucks is bringing together all of the Daimler Group’s fuel-cell activities in a new fuel-cell entity and will place them in the planned joint venture. This also includes the allocation of the operations of Mercedes-Benz Fuel Cell GmbH to Daimler Truck AG.
Press photos are available for download from
https://www.mtu-solutions.com/eu/en/news-and-media/media-center.html
About Rolls-Royce Holdings plc
1. Rolls-Royce pioneers cutting-edge technologies that deliver clean, safe and competitive solutions to meet our planet’s vital power needs.
2. Rolls-Royce Power Systems is headquartered in Friedrichshafen in southern Germany and employs more than 10,000 people. The product portfolio includes mtu-brand high-speed engines and propulsion systems for ships, power generation, heavy land, rail and defence vehicles and for the oil and gas industry as well as diesel and gas systems and battery containers for mission critical, standby and continuous power, combined generation of heat and power, and microgrids. Medium-speed engines from Bergen power ships and power generation applications.
3. Rolls-Royce has customers in more than 150 countries, comprising more than 400 airlines and leasing customers, 160 armed forces, 70 navies, and more than 5,000 power and nuclear customers.
4. Annual underlying revenue was £15.3 billion in 2019, around half of which came from the provision of aftermarket services.
5. In 2019, Rolls-Royce invested £1.45 billion on research and development. We also support a global network of 29 University Technology Centres, which position Rolls-Royce engineers at the forefront of scientific research.
6. The Group has a strong commitment to apprentice and graduate recruitment and to further developing employee skills.
For further information, please contact:
Daimler Truck AG:
Uta Leitner
+49 (0) 711 17-5 30 58
uta.leitner@daimler.com
Peter Smodej
+49 (0) 711 17-5 32 30
peter.smodej@daimler.com
| Phone: | +49 7541 90 2159 | 
| E-mail: |