Rolls-Royce Expands mtu Power Generation Footprint in Mankato
Posted on October 13, 2020
Rolls-Royce has announced a $13.9m investment in its Power Systems business unit for the addition of a new research and development building and multi-phase expansion of its mtu power generation manufacturing facility in Mankato, Minnesota, USA.
- Increased customer demand and industry outlook drive need for increased capacity in the Americas
 - Multi-phase expansion to provide added production lines, increased testing capabilities and additional manufacturing jobs
 
Rolls-Royce has announced a $13.9m investment in its Power Systems business unit for the addition of a new research and development building and multi-phase expansion of its mtu power generation manufacturing facility in Mankato, Minnesota, USA. The project is a result of growth in the market – 2019 was a record year for the Mankato facility – and demand for increased product offerings resulting in the need for updated facilities, equipment and processes to safely handle customer requirements. It is also part of the ongoing journey of Power Systems towards the development of sustainable solutions.
The main portion of the Mankato expansion will be the addition of 28,000-sq-ft to the facility’s existing assembly hall, allowing for additional assembly lines, enhanced product testing capabilities and the creation of 20 new manufacturing positions. By expanding one of the existing assembly lines to accommodate the production of high-power mtu gas generator sets, capacity at the plant is expected to increase by an estimated 25%. This will mark the first time these gas generator sets have been produced in the US.
“Our mtu plant in Mankato has played a decisive role in our encouraging growth in the Americas. We intend to continue on this successful course by working hard to emerge from the crisis stronger than before. More consistently than before, we are pursuing our strategy of evolving from an engine manufacturer to a provider of sustainable solutions," said Andreas Schell, CEO of Rolls-Royce Power Systems. "This investment in our Mankato plant will help us to meet the growing demand for energy in the Americas with locally manufactured products. Mankato will thus become an even more important part of our worldwide production network in the future," Schell continued.
“Rolls-Royce has made significant investments in the gas systems business in terms of both products and people,” said Carsten Schrick, Director for Gas Sales in the Americas. “We have seen an uptick in gas systems projects as a result and we expect that trend to continue, especially as our mtu systems can increasingly run on a variety of gases and offer fuel flexibility. When these systems are available from our plant in Mankato, we will be able to deliver them with shorter lead times to our customers in the Americas, which will be a great benefit for our customers.”
A final benefit of the expansion project is that it will allow for improved logistics services and safety enhancements to the site. With the added space, logistics will be separated from assembly operations, and oversized doors will be added to better facilitate lifting and rigging operations. The traffic routes and parking for the site will also be modified to separate truck traffic from employee parking.
Along with the facility expansion, the overall project investment includes the addition of a new research and development building, upgraded production test cells and the remodeling of the facility’s front office administration area. The new R&D center, which will be fully operational this month, will include a dedicated test cell to meet customer-testing requirements for products going into data center applications. The three production test cells in the main facility will be upgraded to meet these same criteria for testing production units. The front office renovation was completed in December 2019 and included the addition of 21 new workstations.
The first phase of the assembly hall expansion is set to be complete in February 2021, with the final phase targeted for completion in September 2021.
About Rolls-Royce Holdings plc
- Rolls-Royce pioneers cutting-edge technologies that deliver clean, safe and competitive solutions to meet our planet’s vital power needs.
 - Rolls-Royce Power Systems is headquartered in Friedrichshafen in southern Germany and employs around 10,000 people. The product portfolio includes mtu-brand high-speed engines and propulsion systems for ships, power generation, heavy land, rail and defence vehicles and for the oil and gas industry as well as diesel and gas systems and battery containers for mission critical, standby and continuous power, combined generation of heat and power, and microgrids. Medium-speed engines from Bergen power ships and power generation applications.
 - Rolls-Royce has customers in more than 150 countries, comprising more than 400 airlines and leasing customers, 160 armed forces, 70 navies, and more than 5,000 power and nuclear customers.
 - Annual underlying revenue was £15.45 billion in 2019, around half of which came from the provision of aftermarket services.
 - In 2019, Rolls-Royce invested £1.46 billion on research and development. We also support a global network of 29 University Technology Centres, which position Rolls-Royce engineers at the forefront of scientific research.
 
| Phone: | 
           +1 248 560 8488 
         | 
      
| E-mail: |