Rolls-Royce secures emergency backup power for colocation data centre in Colorado with mtu Kinetic PowerPacks
Posted on June 06, 2024
- Kinetic energy system provides immediate response in case of outage or power disruption from grid
- Colorado Springs location to be pilot for possible future expansion
Rolls-Royce has received an order from its distributor Smith Power Products to provide two 1,500kW mtu Kinetic PowerPacks (KPPs) for NOVVA Data Centers, the pioneers of sustainable, secure colocation in the Western United States. The two KPPs will provide emergency backup power for an expansion at the company’s Colorado Springs data center. The Power Systems division of Rolls-Royce has already delivered over 50MW of mtu emergency diesel gensets for NOVVA’s various locations through Smith Power Products.
NOVVA Data Centers places a strong emphasis on conservation and sustainability, so choosing a backup power system that fit this vision was also a significant consideration. The KPP’s battery-free design and ability to run on hydrotreated vegetable oil (HVO)/ renewable diesel fits in perfectly with NOVVA’s environmental approach. Additionally, Smith Power will be providing a selective catalytic reduction (SCR) system to nearly eliminate the emission of nitrogen oxides when the system is running. Also included in the scope of supply are custom enclosures for the units, including 24-hour fuel storage.
Unlike static UPS systems where batteries are required to pick up the immediate load before the diesel engine fires up, the KPP is considered a dynamic UPS system. It uses stored kinetic energy from the flywheel to power the synchronous machine and provide an immediate response until the engine comes online seconds later to take over the load.
Nick Paolo, Business Development Manager, Smith Power Products said: “The space and cost savings from the battery-free design of the KPP system were key considerations for NOVVA in deciding on this solution for an expansion at their Colorado Springs location. We have already installed over 50MW of emergency standby power for NOVVA’s various locations based on mtu Series 4000 gensets, so we’re excited to demonstrate the same absolute reliability the KPP technology has to offer.”
The KPPs will be built at the Rolls-Royce competence center in Liege, Belgium and are scheduled to be commissioned in Q4 2024. They will be supported locally by a full-service maintenance contract to ensure the system performs at the highest level for its 20+ year lifecycle.
To learn more about mtu Kinetic PowerPacks, visit mtu Kinetic PowerPack (mtu-solutions.com)
About Rolls-Royce Holdings plc
- Rolls-Royce is a force for progress; powering, protecting and connecting people everywhere. Our products and service packages help our customers meet the growing need for power across multiple industries; enable governments to equip their armed forces with the power required to protect their citizens; and connect people, societies, cultures and economies together.
- Rolls-Royce has a local presence in 47 countries and customers in over a hundred more, including airlines and aircraft leasing companies, armed forces and navies, and marine and industrial customers.
- Through our multi-year transformation programme, we are building a high-performing, competitive, resilient and growing Rolls-Royce. We are building the financial capacity and agility to allow us to successfully develop and deliver the products that will support our customers through the energy transition.
- Annual underlying revenue was £20.1 billion in 2025, and underlying operating profit was £3.46 billion.
- Rolls-Royce Holdings plc is a publicly traded company (LSE: RR., ADR: RYCEY, LEI: 213800EC7997ZBLZJH69).
- Rolls-Royce Power Systems is headquartered in Friedrichshafen in southern Germany and employs more than 10,350 people. The product portfolio includes mtu-brand high-speed engines and propulsion systems for ships, heavy land, rail and defence vehicles and for the oil and gas industry. The portfolio also includes diesel and gas systems and battery containers for mission critical, standby and continuous power, combined generation of heat and power, and microgrids. With its climate friendly technologies, Rolls-Royce Power Systems is helping to drive the energy transition.
Contact
| Phone: |
+1 248 560 8488
|
| E-mail: |