STORY

How does Common Rail Injection work?

Posted on June 24, 2014 by Dr. Johannes Kech, Images by mtu

Common rail injection allows the combustion process to be optimized so that less pollutant is produced from a smaller amount of fuel.
Friedrichshafen, Germany

With common rail fuel injection, the combustion process can be optimized to achieve low pollutant levels combined with lower fuel consumption. Fuel is injected into the combustion chamber from a common rail under high pressure. The electronic control system ensures that the start of injection, the quantity and time are independent of the engine speed. In 1996, with the Series 4000 engine, mtu was the first manufacturer of large diesel engines to introduce common rail fuel injection as a standard feature.

Pioneer of the common rail fuel injection system                                                 The emissions regulations for diesel engines in applications such as ships, trains and heavyduty off-road vehicles and gensets worldwide are becoming more stringent and make extensive modifications to the power units necessary. At the same time, customers are constantly calling for more economical engines. Exhaust after treat-ment systems such as SCR catalytic converters (selective catalytic reduction, short: SCR) or diesel particulate filters are one way of lowering emissions, but also have a greater space requirement and potentially increase the engine’s maintenance needs. For these reasons, mtu primarily pursues a policy of reducing emissions by internal engine enhancements. Fuel combustion inside the engine is improved so that, if at all possible, emissions are not produced in the first place. If necessary, mtu introduces a second phase of emission control whereby remaining harmful emissions are removed by exhaust aftertreatment systems.

Fig. 1: Common rail system for Series 4000 The performance and flexibility of the CR system create the prerequisites for clean and efficient combustion.

As part of the internal engine enhancements, one of the major means of control for obtaining clean fuel combustion, besides exhaust gas recirculation, is the fuel injection system. It is designed to inject the fuel at high pressure at precisely the right moment, while also accurately metering the quantity of fuel injected in order to create the conditions required for lowemission combustion inside the cylinder. With precise control of fuel volume delivery at high pressure, fuel consumption can also be dramatically reduced. This is the reason why mtu implemented a technology change from conventional mechanical injection systems to the flexible, electronically controlled common rail system at a very early stage — at the time mainly with a view to producing more economical engines. In 1996, mtu equipped the Series 4000, the first large diesel engine, with a common rail system as a standard feature. A common fuel pipeline — the so-called rail that gives the system its name — supplies all the engine’s fuel injectors with fuel. When fuel is to be injected into a cylinder, the system opens the nozzle of the relevant injector and the fuel flows from the rail into the combustion chamber, is atomized by the high pressure in the process, and mixes with the air. The common rail system components have to be extremely precisely and flexibly controlled. For this purpose, mtu uses its ECU (Engine Control Unit, see Figure 1), a proprietary engine management system that was developed in-house. Due to the increasingly stringent emissions standards for engines of all power classes and all types of application, mtu in future will be fitting all newly developed engines with common rail fuel injection.

Lower emissions due to combination with other key technologies


With combustion optimization by internal engine design features there is a three-way interaction between nitrogen-oxide formation, the production of soot particulates and fuel consumption: the more intensive the combustion and thus the energy conversion, the lower the particulate emissions and consumption and the higher the nitrogen oxide emissions. Conversely, retarded combustion leads to lower nitrogen oxide formation,
but also to higher fuel consumption and particulate emission levels. The job of the engine developers is to find a compromise between these extremes for every point on the engine performance map. When doing so, they must harmonize the effect of the fuel injection system with that of other internal engine measures such as exhaust gas recirculation, which primarily reduces nitrogen oxide emissions, and external exhaust aftertreatment systems. As a pioneer in this field, mtu can draw from many years of experience with fuel injection systems produced by Rolls-Royce Power Systems brand L’Orange and other suppliers. In the course of this period, mtu has acquired comprehensive expertise in the integration of the common rail fuel injection system into the engine. This has enabled the company to fully utilize the potential of the fuel injection system in combination with other key technologies for refining the combustion process. The two key parameters in fuel injection that affect fuel consumption and emissions are injection rate and injection pressure.
Fig. 2: Fuel flow and injection sequence for multiphase injection mtu divides the fuel injection sequence into as many as three separate phases. The main injection phase delivers the fuel, a preinjection phase reduces the load on the crankshaft drive gear, and a post-injection phase reduces particulate emissions. This enables both fuel consumption and emissions to be reduced.

Injection rate: pre-, main and post injection


The injection rate determines when and how much fuel is injected into the cylinder. In order to reduce emissions and fuel consumption, the present evolution stage of the injection system for mtu engines divides the fuel injection sequence into as many as three separate phases (see Figure 2). The timing of the start of injection, the duration and amplitude are userdefined in accordance with engine performance map. The main injection phase supplies the fuel for generating the engine’s power output. A preinjection phase initiates advance combustion to provide controlled combustion of the fuel in the main injection phase. This reduces nitrogen oxide emissions, because the abrupt combustion prevents high peak temperatures. A post injection phase shortly after the main injection phase reduces particulate emissions. It improves the mixing of fuel and air during a late phase of combustion to increase temperatures in the combustion chamber, which promote soot oxidation. Depending on the engine’s operating point, the main injection phase can be supplemented as required by including pre- and/or post injection phases.
Comparison of injector sizes for engines with different cylinder capacities, including injectors for the current mtu Series 1600, 2000, 4000 and 8000 engines. (light grey: non-mtu engines)

Injection pressure: peak pressures of up to 2,200 bar


Injection pressure has a significant influence on particulate emission levels. The higher the injection pressure, the better the fuel atomizes during injection and mixes with the oxygen in the cylinder. This results in a virtually complete combustion
of the fuel with high energy conversion, during which only minimal amounts of particulates are formed. For this reason, mtu has continually raised the maximum injection pressure of its common rail systems from 1,400 bar in the case of the Series 4000 engine in 1996 to the present 2,200 bar for the Series 1600, 2000 and 4000 engines (see Figure 3). In the case of the Series 8000 engine, it is 1,800 bar. For future engine generations, mtu is even planning injection pressures of up to 2,500 bar. Over the same period, mtu has further improved the system’s durability and ease of maintenance. A filter concept designed to meet the requirements has further improved the injection system’s ability to cope with particle contamination in the fuel. In future, injector servicing intervals will be extended with the aid of electronic diagnostics.
Fig. 3: Change in injection pressures since 1996 for Series 4000 engines Since 1996, mtu has steadily increased the injection pressures to further reduce consumption and particulate emissions. Since 2000, mtu has used advanced versions of the common rail system on the Series 4000, amongst others, in which each fuel injector has its own fuel reservoir. The advantage is that even with large injection quantities, the fuel rail remains free of pressure fluctuations and the injection sequences of the individual cylinders do not interfere with each other.

Solo system: injectors with their own fuel reservoir


Because of its performance capabilities, the common rail injection system has established itself as standard equipment on car diesel engines in the course of the last few years. The version of the system as described is also well suited for use in small capacity industrial engines. In the case of engines with larger cylinder capacities, however, the conventional common rail system is now revealing its limitations, since these require a relatively large quantity of fuel to be injected into the cylinder for each ignition stroke. This produces pressure pulsations in the common rail system’s fuel reservoir that can interfere with the subsequent injection sequences. Since 2000, mtu has used an advanced version of the common rail system for the Series 4000 and 8000 engine, and since 2004 for the Series 2000 as well, in which the fuel injectors have an integrated fuel reservoir (see Figure 4). This permits the fuel lines between the injectors and the common rail to have a relatively small cross section. During an injection sequence, all that happens is that the pressure in the injector’s own fuel reservoir drops slightly. This prevents pressure fluctuations in the common rail system and, therefore, a momentary undersupply or oversupply of fuel to the injectors.
Fig. 4: Injector with integrated fuel reservoir The use of injectors with an integrated fuel reservoir prevents pressure fluctuations in the common rail system and, therefore, a momentary undersupply or oversupply of fuel to the injectors.

Tailored solutions for flexible use of fuel


With the higher technical performance levels of the injection systems, the demands placed on the fuel in terms of purity and quality also rise. Thus the fuel must comply with pre-defined values for viscosity and lubricity, as components of the highpressure
pumps and injectors are lubricated by the fuel. It must also be free of any contam-ination that would lead to abrasive damage at the high pressures employed. To ensure that the engine operates correctly, therefore, only diesel fuel that is approved for the application in question and meets the applicable standard may be used. At the customer’s request, mtu carries out analyses for specific application-related approval of other fuels in close cooperation with Rolls-Royce Power Systems brand L’Orange or alternative suppliers. With some applications, for example, a lack of lubricating
properties on the part of the fuel can be compensated for by special coatings on the injection system. In addition, mtu assists customers when designing the onsite tank and fuel system. This is of great interest for mining vehicles, for instance, that are subjected to high levels of dust exposure.

Summary


mtu continually develops its engines to ensure they will meet the tough future emissions standards, while at the same time consuming as little fuel as possible. To this end, mtu optimizes fuel combustion in the cylinder by means of its electronically controlled common rail fuel injection system in combination with other technologies such as exhaust gas recirculation. By achieving clean and efficient combustion, the expense of exhaust aftertreatment systems can be minimized and, in some cases, eliminated altogether. mtu has used common rail systems success fully since as long ago as 1996 and has continually advanced the technology in collaboration with Rolls-Royce Power Systems brand L’Orange and other suppliers. Due to its extensive expertise in common rail injec -tion systems, mtu is able to optimally exploit the potential of the technology in order to make engines extremely economical and clean.

Point of contact

Dr Johannes Kech
Phone:
+49 7541 90 2153
E-mail:

Related stories

How does Exhaust Gas Recirculation work?

by Dr. Johannes Kech

To reduce nitrogen oxide emissions, a proportion of the exhaust gases is cooled and then reintroduced into the charge-air.

Read more

How does a Diesel Particulate Filter work?

by Gudio Schäffner

Diesel particulate filters can be used to remove most of the soot particles from diesel engine exhaust gases.

Read more

How does Selective Catalytic Reduction work?

by Dr. Holger Sinzenich

Selective catalytic reduction employs chemical reduction to render nitrogen oxides harmless.

Read more

Turbocharging: Key technology for high-performance engines

by Dr. Johannes Kech

Turbochargers give engines their power and their unmistakable character.

Read more