PRESS RELEASE Power Generation

Rolls-Royce introduces fast-start mtu gas gensets for powering data centers

Posted on October 01, 2025

Images [2 Files, 3 MB]

  • New from 2026: 20V4000 mtu gas generator as a 45-second fast-start solution for the U.S. market
  • Already available globally: all mtu gas generators as 120-second fast-start solutions
  • New portfolio supports growing energy demand of AI data centers and stability of power grids

Rolls-Royce is expanding its energy portfolio with new mtu gas engines that feature fast-start capability, making them particularly suitable for powering data centers and stabilizing the power grid. Starting in 2026, the new 20-cylinder mtu Series 4000 L64 engine for the 60 Hz market (primarily North America), will be able to deliver its full output of 2.8 Megawatts in just 45 seconds. Performance has been increased by ten percent compared to the previous version. The latest version does not require a gearbox, which means significant space savings for data center operators. Current versions of the mtu Series 4000 gas gensets for both 50 Hz and 60 Hz are already available worldwide with a fast-start capability of 120 seconds.

 “We expect that natural gas will increasingly be used to meet the growing energy demands of (AI) data centers in the future, particularly in North America, where it is relatively inexpensive and readily available. This 45-second fast-start solution with higher power output will represent a significant advancement for our customers and their ability to secure power for their operations,” said Kevin McKinney, Vice President Powergen Sales Americas at Rolls-Royce Power Systems.

 The fast-start mtu gas gensets can be used in data centers for emergency power supply, but also for continuous power supply and in combination with mtu diesel gensets. The continuous power application is especially attractive when the existing grid power is not sufficient to take on the new load of a data center coming online. By using an independent gas power plant, operators may be able to come online faster and realize other benefits such as increased energy security and additional revenue from feeding electricity into the grid. mtu Series 4000 natural gas generators offer the advantages of long life – boasting 84,000 hours before overhaul and are available in a container version. 

Gas units can reduce emissions such as nitrogen oxides and CO2 and improve efficiency when generating electricity and heat or cooling. mtu gas engines can be operated with sustainable fuels such as biogas and biomethane, and as soon as green hydrogen becomes available, they can also be operated with 100 percent hydrogen or with a hydrogen admixture.

“Especially since the energy consumption of data centers worldwide will double by 2030, our customers will need solutions from us that are efficient, sustainable, and secure. This is the reason why we are continuing to invest heavily in expanding our portfolio and as well in different technologies to offer our customers the best solutions for today’s but also for future requirements.” explained Tobias Ostermaier, President Stationary Power Solutions at Rolls-Royce Power Systems.

mtu gas gensets are already being used to supply power to data centers. SpaceDC, for example, operates its data center campus in Jakarta using Rolls-Royce technology. mtu gas and diesel systems with exhaust gas aftertreatment technology ensure efficient and clean base load and emergency power supply as well as cooling.

In times when power grids are under strain due to the connection of large data centers and the integration of volatile renewable energies, modular gas power plants can help to ensure security of supply. mtu gas engines already provide reliable power and heat supply worldwide: In Alberta, Canada, they support the power grid during peak loads to ensure continuous availability. In the UK, a fleet of more than 500 mtu gas gensets is already in operation.

Please see further information on the mtu data center solutions here:

AI boom: How combustion engines secure the power
supply for data centers – and what Rolls-Royce is planning next

https://www.mtu-solutions.com/eu/en/applications/power-generation/power-generation-applications/data-centers.html

About Rolls-Royce Holdings plc

  1. Rolls-Royce is a force for progress; powering, protecting and connecting people everywhere. Our products and service packages help our customers meet the growing need for power across multiple industries; enable governments to equip their armed forces with the power required to protect their citizens; and connect people, societies, cultures and economies together.
  2. Rolls-Royce has a local presence in 47 countries and customers in over a hundred more, including airlines and aircraft leasing companies, armed forces and navies, and marine and industrial customers.
  3. Through our multi-year transformation programme, we are building a high-performing, competitive, resilient and growing Rolls-Royce. We are building the financial capacity and agility to allow us to successfully develop and deliver the products that will support our customers through the energy transition.
  4. Annual underlying revenue was £20.1 billion in 2025, and underlying operating profit was £3.46 billion.
  5. Rolls-Royce Holdings plc is a publicly traded company (LSE: RR., ADR: RYCEY, LEI: 213800EC7997ZBLZJH69).
  6. Rolls-Royce Power Systems is headquartered in Friedrichshafen in southern Germany and employs more than 10,350 people. The product portfolio includes mtu-brand high-speed engines and propulsion systems for ships, heavy land, rail and defence vehicles and for the oil and gas industry. The portfolio also includes diesel and gas systems and battery containers for mission critical, standby and continuous power, combined generation of heat and power, and microgrids. With its climate friendly technologies, Rolls-Royce Power Systems is helping to drive the energy transition.

www.rolls-royce.com

Contact

Silke Rockenstein Spokeswoman Trade Media
Phone:
+49 7541 90 7740
E-mail: