Combination of trimaran concept and mtu engines is convincing
David Singleton, Austal's CEO, said that the results of the Bajamar Express' trials, during which a speed of over 44 knots was achieved, exceeding the contract speed, were a great demonstration of the trimaran's unique capabilities and exceptional seakeeping characteristics. "In 2005 we at Austal implemented a successful trimaran concept for Fred Olsen with the Benchijigua Express. The new generation of high-speed ferries, builds on this concept and will provide an even greater customer experience".
Impact of Covid-19
The Bajamar Express and its sister ship Bañaderos Express, which is under construction, have all the preventive measures for safety in accordance with Covid-19, and the company and its protocols are also certified by the Spanish company Aenor. "We are very proud that Fred. Olsen Express is the first Spanish transport and tourism company to receive this important certification," said Andrés Marín, CEO of Fred. Olsen S.A. A crew of 19 persons from Fred. Olsen spent 14 days in quarantine after entering Australia due to the Covid 19 pandemic before they could take over the trimaranfor the crossing.
"The entire Fred-Olsen-Express team can hardly wait for the Bajamar Express to arrive in the Canary Islands." The sister ship, the Bañaderos Express, will follow in the first half of 2021.
12 engines of series 8000 in service
These new vessels will join the Benchijigua Express trimaran in the Canary Islands, which has been running with mtu 20V 8000s since 2005. All three vessels will have be covered by a maintenance contract from mtu.