Spanish map, dramatic stormy clouds with electrical wiring, blackout in Spain
STORY Power Generation

standby power generators: The back-up for the worst case scenario

Posted on May 22, 2025

mtu standby power generators are in demand like never before. What they can do, where to find them and what their climate-neutral future looks like.
Friedrichshafen, Germany
At the end of April 2025, the Iberian Peninsula experienced one of the most significant power failures in recent memory. At approximately 12:30 p.m., the Spanish electricity grid lost 15 gigawatts of generation—likely renewable—in a sudden five-second collapse. The blackout impacted over 53 million people across Spain and Portugal, with ripple effects reaching into southern France. Amid widespread outages, critical infrastructure held steady. Data centers remained online, airport systems stayed operational, and key services were uninterrupted— also thanks to mtu standby generators and Kinetic Powerpacks from Rolls-Royce.

Growing demand for mtu solutions: Global energy demand on the rise 

From airports and hospitals to data centres or companies with particularly sensitive production processes, such as the semiconductor or pharmaceutical industry: Electricity must never be absent. That is why mtu standby power generators are often found in these facilities. As soon as the public power supply is no longer sufficient or is interrupted, the diesel gensets take over and supply the necessary power. Accordingly, the requirements for the standby power supply are extraordinarily high. "Rolls-Royce is at home in this segment," says Dennis Zumbach, Sales Director Power Generation in Europe, Africa and the Middle East at Rolls-Royce's Power Systems Division.      

The demand for standby power generators is currently booming like never before. "The biggest driver is mainly the data centre industry which requires full capacity utilization," explains Zumbach.

The reason for this is the steadily increasing energy demand of data centres. With video streaming, Industry 4.0 and growing AI requirements, the demand for computing power has increased massively over the last years. 

mtu standby power units: from data centre to hospital

This is why many mtu standby power units can be found in data centres and other critical industries. For example, AVK, as the largest supplier of standby power solutions in the UK, has been working exclusively with Rolls-Royce for over 20 years and has in the meantime delivered and installed several hundred mtu standby power units of the 2000 and 4000 series.

AVK, as the largest supplier of standby power solutions in the UK, has been working exclusively with Rolls-Royce for over 20 years and has in the meantime delivered and installed several hundred mtu standby power units of the 2000 and 4000 series.
Hospitals such as the famous Charité in Berlin have also had two Rolls-Royce gensets in a purpose-built building since 2010. In addition to two diesel gensets with mtu 12V 4000 G23 engines, Rolls-Royce also supplied the cooling, fuel and exhaust systems, the supply and exhaust air system and the control system - in other words, a complete turnkey system. With an electrical output of 850 kVA per unit, the Charité can be supplied with standby power for around 50 hours.
Our mtu emergency gensets will provide reliable backup power for the European Commission's new Jean Monnet 2 building complex in Luxembourg. They will ensure that all essential and safety-related equipment within the buildings, as well as their technical systems, can continue to operate without interruption in the event of a power outage.
Six Series 4000 diesel gensets, each delivering 2560 kW, ensure a total of 15 MW backup power for Start Campus’s hyperscale data center in Sines, Portugal. As one of Europe’s greenest campuses, it runs on 100% renewable energy and leverages advanced seawater cooling. To align with its sustainability goals, the mtu emergency gensets are powered by HVO—an eco-friendly fuel choice that supports a cleaner, more resilient energy future.

What can mtu standby power generators do?

Whether in the freezing cold of Siberia or during an earthquake in North America: mtu standby power generators must work reliably. In California, for example, the earth can shake up to 10,000 times a year, while the standby generator has to function perfectly. On a special test stand, the mtu gensets were tested under conditions similar to an earthquake.    

Uninterruptible power supply: The mtu Kinetic PowerPack

Particularly impressive: The gensets can start extremely quickly. After just a few seconds, the diesel gensets are working at full speed and take over the complete power supply of a plant. The short interim period is bridged by batteries or kinetic mass storage to guarantee an uninterrupted power supply.

Kinetic mass storage devices? They are an essential component of dynamic UPS (uninterruptible power supply) technology. This technology, which at Rolls-Royce is called mtu Kinetic PowerPack, consists of a diesel engine coupled via an electromagnetic clutch to a kinetic energy storage device - in simple terms, a flywheel weighing several tonnes. The mtu Kinetic PowerPacks guarantee a reliable and environmentally friendly uninterruptible power supply and energy processing without batteries.

During normal operation, the kinetic energy storage compensates for current and voltage fluctuations, which can cause problems with highly sophisticated and sensitive IT equipment and consequently lead to major financial losses, among other things. Even if the primary power source fails completely, the stored kinetic energy is sufficient to bridge the time until the diesel engine is running at full speed. 

Pharma service provider Vetter has been relying on our dynamic uninterruptible power supply systems since 2005: nine mtu Kinetic PowerPacks are currently in operation at various company sites, with two more currently being installed. The group uses them to secure the power supply for its production processes.
Rolls-Royce has supplied and commissioned four of its mtu Kinetic PowerPacks to X-FAB Sarawak, the Malaysian division of X-FAB, the world's leading foundry group for specialty semiconductor applications.
mtu Kinetic PowerPacks, manufactured in Liège, Belgium, combine a kinetic energy storage system, an mtu diesel engine and a generator. When the utility grid is operational, the kinetic energy storage device – in this case a flywheel – is driven by the generator, which in this operating mode functions as an electric motor. The heavy kinetic energy storage device serves as an ‘energy battery’ that stores energy and makes it available instantaneously if the power from the main grid fails.

Sustainable standby power supply with HVO, hydrogen and Co.


The demand for climate-neutral solutions is also increasing for the standby generator market. Rolls-Royce is taking concrete steps in this direction. 

A milestone on this path is the already completed approval of mtu engines for use with sustainable fuels of the EN15940 standard. This includes HVO (Hydrotreated Vegetable Oil), which is produced on the basis of vegetable and animal fats, often from waste, not from plants grown specifically for this purpose. HVO can reduce particulate emissions by up to 80 percent and CO2 emissions by up to 90 percent. 

"The great thing about HVO is that you can use the fuel in our engines without limiting performance. Especially in England, many data centres have already converted to using HVO," says Dennis Zumbach.

With our various mtu backup power solutions, the worst-case scenario can become just another routine test passed.

STORY Power Generation

How do gas engines differ from diesel engines?

Gas engines are experiencing a boom. A look under the hood reveals what sets them apart from diesel engines.

Read more

STORY Power Generation

When the Grid Can’t Keep Up: Powering the AI Era

The AI boom is driving global energy demand to unprecedented levels. Find out why grid capacity is increasingly becoming a bottleneck and how mtu solutions are helping pave the way for a digital future.

Read more

STORY Energy Storage

When the wind falls silent and the sun goes to sleep

On the role of battery storage and gas-fired power plants in the energy transition.

Read more

STORY Power Generation

How decentralized gas power plants are making energy supply more stable

What happens when the wind and sun take a break at the same time – and the grid reaches its limits? Rolls-Royce energy experts show how modular gas engine power plants keep the grid stable – flexibly, decentralized, and cost-efficiently.