PRESS RELEASE Commercial Marine

Early recognition, better support: Rolls-Royce is expanding its remote monitoring service for mtu propulsion systems worldwide

Posted on September 23, 2026

Images [1 Files, 1 MB]

  • Remote monitoring provides valuable insights into the operation of mtu systems and enables the early coordination of targeted measures 
  • An improved service concept ensures rapid response times and high availability, and helps customers operate their plants more reliably and efficiently

Rolls-Royce is further expanding its range of data-driven services. In Arcola, Italy, the company has commissioned a new Remote Monitoring Centre (RMC) for vessels fitted with mtu propulsion systems and for power generation plants. Service experts will initially monitor marine and yacht applications, analyse operational data and support customers in ensuring the availability and performance of their systems. Through continuous analysis, changes in operational behaviour can be identified at an early stage, enabling targeted measures to be devised jointly.

Arcola is the first Remote Monitoring Centre outside Berlin, where remote monitoring has so far focused on battery storage systems and microgrids, and marks the starting point for the global roll-out of the concept.

“With remote monitoring, we are evolving our customer service from merely providing support for specific issues to offering continuous support for our customers. The analysis of operational data creates transparency, helps to identify changes at an early stage and enables better planning of maintenance measures. In this way, we support our customers in operating their systems reliably and efficiently,” explained Andreas Görtz, President of the Mobile & Sustainable Business Unit at Rolls-Royce Power Systems. 

Towards a proactive service with the Remote Monitoring Centre

The aim of remote monitoring is to provide customers with even better support in operating their systems reliably and efficiently. To this end, operational data from networked systems is continuously analysed. This enables changes in operational behaviour to be detected at an early stage, allowing targeted measures to be devised jointly.

If the experts at the Remote Monitoring Centre identify any relevant deviations, they support customers with specific recommendations for action to optimise operations and plan maintenance measures. Depending on requirements, further services such as the supply of spare parts or the deployment of a service engineer can also be coordinated.

“With Remote Monitoring, we combine digital technologies with our many years of on-site service expertise. This enables us to create greater transparency regarding the operation of our systems, provide our customers with more targeted support and help to further increase the availability of their plants,” said Jörn Lindstädt, Senior Vice President Global Service at Rolls-Royce Power Systems.

At the Remote Monitoring Centre in Arcola, specially trained staff are currently monitoring the connected fleets and installations. Two customers – the Italian ferry operator Liberty Lines and the Italian shipyard Overmarine – are already benefiting from the new service. Furthermore, plans are in place to further expand the digital connectivity of additional mtu systems and to extend monitoring in collaboration with Italy’s ‘Guardia di Finanza’.

Global network for remote monitoring planned

Remote monitoring in Arcola forms part of a broader service concept from Rolls-Royce. Each centre supports the customers and installations in its region and can, where necessary, call upon additional specialists in analysis and problem-solving. In addition to the regional Remote Monitoring Centres, Remote Monitoring Hubs (RMHs) are to be established in future, which will provide overarching trend analysis and support the regional centres with more complex issues.

mtu Go forms the digital foundation

The mtu Go platform provides the technological basis for remote monitoring. It enables operational data from connected systems to be made available remotely and used for monitoring purposes. Existing, compatible systems can also be retrofitted to use mtu Go.

Rolls-Royce is gradually developing the monitoring functions further. New functions are first tested in pilot applications and then rolled out for wider use. Insights gained from the operation of connected fleets are incorporated into the further development of analytics and monitoring functions.

About Rolls-Royce Holdings plc

  1. Rolls-Royce is a force for progress; powering, protecting and connecting people everywhere. Our products and service packages help our customers meet the growing need for power across multiple industries; enable governments to equip their armed forces with the power required to protect their citizens; and connect people, societies, cultures and economies together.
  2. Rolls-Royce has a local presence in 47 countries and customers in over a hundred more, including airlines and aircraft leasing companies, armed forces and navies, and marine and industrial customers.
  3. Through our multi-year transformation programme, we are building a high-performing, competitive, resilient and growing Rolls-Royce. We are building the financial capacity and agility to allow us to successfully develop and deliver the products that will support our customers through the energy transition.
  4. Annual underlying revenue was £20.1 billion in 2025, and underlying operating profit was £3.46 billion.
  5. Rolls-Royce Holdings plc is a publicly traded company (LSE: RR., ADR: RYCEY, LEI: 213800EC7997ZBLZJH69).
  6. Rolls-Royce Power Systems is headquartered in Friedrichshafen in southern Germany and employs more than 10,350 people. The product portfolio includes mtu-brand high-speed engines and propulsion systems for ships, heavy land, rail and defence vehicles and for the oil and gas industry. The portfolio also includes diesel and gas systems and battery containers for mission critical, standby and continuous power, combined generation of heat and power, and microgrids. With its climate friendly technologies, Rolls-Royce Power Systems is helping to drive the energy transition.

www.rolls-royce.com

Contact

Silke Rockenstein Spokeswoman Trade Media
Phone:
+49 7541 90 7740
E-mail: