STORY Power Generation

mtu Kinetic PowerPacks: How Dynamic Uninterruptible Power Supply systems work

Posted on October 11, 2023 by Lucie Maluck, Images by Rolls-Royce Power Systems

"Uninterruptible Power Supply Systems" - or mtu Kinetic PowerPacks - are pretty exciting. They are among the most exciting products from Rolls-Royce Power Systems.
mtu Kinetic PowerPacks
Our mtu Kinetic PowerPack provides dynamic uninterruptible power supply through kinetic energy and is engineered to withstand the most demanding power supply challenges.
Read more
What Dynamic Uninterruptible Power Supply Systems do?

Dynamic UPS systems provide perfect conditioned electrical power to critical consumers. In normal operating mode i.e. when the public power grid is available, a choke – an electromagnetic coil is used – to eliminate current and voltage fluctuations that the power grid tends to produce. These voltage fluctuations are actually very frequent but are not perceived by 'normal' consumers. Today's sophisticated IT systems however are increasingly sensitive, and a power grid fluctuation can cause their function to be perturbed. When that happens in a hospital or data center or in factories that run very sensitive production processes, the consequences can be dramatic, and involve huge financial losses.  

mtu diesel engine

Complying with the latest emissions standards; preheated; quick start and not running during conditioning mode pre-lubricated.

Synchronous machine

Four-pole synchronous machines from world-renowned manufacturers designed not to exceed Class F temperature rise; right-sized for your application and to absorb load harmonics.

Kinetic energy module

Patented accu provides stored kinetic energy to ride through mains interruptions; designed for a 10-year bearing life.

Vibration isolation

Thanks to the solid base frame with isolators between frame and equipment and direct floor installation, vibrations are reduced >97% .

Power panel

A power panel comprising input, output and automatic bypass circuits; additional upstream, down-stream or tie-breakers can be added, if required.

Control system

KS Vision HMI control system; class-leading electrical and mechanical monitoring including load level, mains failures, input and output voltage, frequencies and power factor; data logging feature recording all historic events.

Electromagnetic clutch

The prime starter system consists of standard engine starting motors. The clutch is maintenance-free and guarantees the diesel engine to start at all times, thanks to the redundant start feature.

1

mtu diesel engine

Complying with the latest emissions standards; preheated; quick start and not running during conditioning mode pre-lubricated.

2

Synchronous machine

Four-pole synchronous machines from world-renowned manufacturers designed not to exceed Class F temperature rise; right-sized for your application and to absorb load harmonics.

3

Kinetic energy module

Patented accu provides stored kinetic energy to ride through mains interruptions; designed for a 10-year bearing life.

4

Vibration isolation

Thanks to the solid base frame with isolators between frame and equipment and direct floor installation, vibrations are reduced >97% .

5

Power panel

A power panel comprising input, output and automatic bypass circuits; additional upstream, down-stream or tie-breakers can be added, if required.

6

Control system

KS Vision HMI control system; class-leading electrical and mechanical monitoring including load level, mains failures, input and output voltage, frequencies and power factor; data logging feature recording all historic events.

7

Electromagnetic clutch

The prime starter system consists of standard engine starting motors. The clutch is maintenance-free and guarantees the diesel engine to start at all times, thanks to the redundant start feature.

How does a dynamic UPS system work? 

mtu Kinetic PowerPacks comprises a constantly rotating kinetic energy storage unit with flywheel, an mtu diesel engine and an alternator which, depending on the operating mode, also operates as an electric synchronous motor with its preferred compensation characteristics. A special control unit with the accompanying switchgear and a choke that acts as a line filter, complete the system. Power from the public grid drives the synchronous alternator, which acts as an electric motor in this operating mode. This in turn drives the flywheel in the kinetic energy storage unit which weighs tons and is designed as an electric machine with double rotor system. This serves as the 'energy accu' which stores energy and makes it available in the unlucky event of a power outage.

 

Youtube Video

What happens when the primary power source fails?

If the public power grid fails, the mtu Kinetic PowerPack acts immediately and without interruption because it is already in operation anyway. Part of the energy stored in the flywheel is used to drive the generator, that starts producing electrical power. Meanwhile, another part of the stored rotational energy is used to facilitate very fast start-up of the diesel engine. Within the shortest possible time the engine accelerates to its rated power output and can now start producing electrical power via the generator and stabilize the flywheel. This naturally happens without any gap or interruption – hence the name 'Uninterruptible Power Supply'.  

Is another battery required?

No. With mtu Kinetic PowerPacks, no battery is required. Previously, Rolls-Royce only had mtu standby generator sets in its portfolio for dealing with power outages. These require a certain amount of time to get going, however. To bridge that gap and ensure an uninterrupted flow of power, customers have often resorted to batteries. In mtu Kinetic PowerPacks, however, no such battery is needed, since the energy in the kinetic energy storage unit can be made available immediately for generating power until the mtu diesel engine comes on-line. 

What happens precisely?

Well - here's an explanation for the expert or anyone wishing to become one: The flywheel – essentially a kinetic energy accumulator – forms the heart of the system. The flywheel consists of two rotating elements: an outer rotor running freely around an inner rotor which is driven by the main shaft and rotates at 1,500 rpm (50 Hz) or 1,800 rpm (60 Hz). It has two sets of windings: a three-phase alternating current (AC) winding and a direct current (DC) winding.When the public power grid is available, the AC winding is energized to create a rotating magnetic field that drives the outer rotor at a maximum speed of 3,000 rpm. However, the relative speed between the inner and outer rings of the bearings is only 1,500 rpm, since the shaft itself rotates at 1,500 rpm. The external rotor stores kinetic energy advantageously, since the amount of kinetic energy increases by the square as the distance from the center of rotation increases.

In conditioning mode, when the mains supply is within tolerance, the synchronous machine is acting as a motor, driving the main shaft and thus the accu, storing kinetic energy in it. When the inner rotor rotates at 1500 rpm (50 Hz) or 1800 rpm (60 Hz), the outer rotor then rotates at maximum 3000 rpm. The kinetic energy is thus stored.

During a mains failure when the system is supplying emergency power, the DC winding is fed and the outer rotor is electrically coupled to the inner rotor by induction. Its kinetic energy is transferred to the inner rotor – driving it. This energy transfer is regulated by precise control of the current fed into the DC winding. The accumulator for the kinetic energy is an entirely brushless system.

During mains failure or voltage perturbation the stored kinetic energy is now transferred to the kinetic energy accumulator, which acts as a generator. This happens without any interruption to the user. Shortly after, the diesel engine starts and couples to the kinetic energy accu by latching the electromagnetic clutch. The energy is then relayed from the diesel engine to the synchronous machine and then to the loads.
Energy Storage

When the wind falls silent and the sun goes to sleep

by Lucie Maluck

On the role of battery storage and gas-fired power plants in the energy transition.

Read more

Power Generation

How decentralized gas power plants are making energy supply more stable

by Lucie Maluck

What happens when the wind and sun take a break at the same time – and the grid reaches its limits? Rolls-Royce energy experts show how modular gas engine power plants keep the grid stable – flexibly, decentralized, and cost-efficiently.

Read more

Power Generation

AI boom: How combustion engines secure the power supply for data centers – and what Rolls-Royce is planning next

by Silke Rockenstein

Rolls-Royce has the most comprehensive portfolio for powering data centres – from diesel generators to SMR.

Read more

Power Generation

From the tap to the future: How COâ‚‚ is becoming a valuable resource

by Lucie Maluck

What makes beer fizzy today was exhaust gas yesterday: in Worksop, Rolls-Royce and its partners are demonstrating how COâ‚‚ is breaking new ground as a resource.

Read more

Connect with Us

Customer Assistance Center

We are here to take your Sales & Service questions around the clock, 365 days a year.

Read more

Sales & Service Locator

Find your local partner for Sales & Service.

Read more

mtu Stories

Reports and interviews about mtu products and solutions.

Read more