MTU-Motoren gibt es in allen Farben, die die Kunden sich wünschen. Doch wie werden die Motoren farbig? Ein Blick in die Lackiererei.
STORY

How do we do... colors?

Posted on May 12, 2014, Images by Robert Hack

mtu engines come in whatever color the customer wants. But how are they finished? A look behind the scenes in our paint shop.
Friedrichshafen, Germany
Before the engine can be sprayed, a paintshop technician has to mask off all parts that are not to be painted.
The engine is towed to the drying booth on a trailer. There, it is fanned by dehumidified air at a temperature of 60 degrees.

Point of contact

Dominik Hülsbusch
Phone:
+49 7541 90 8599
E-mail:

Related stories

How do we make... a crankcase?

The crankcase forms has to be able to withstand immense forces. That is why it is built to tolerances of just a few hundredths of a millimeter.

Read more

How to make a... cylinder head?

CAD, machining center, assembly line: the three main stages of cylinder head production.

Read more

How do we make... metal harder?

1,800 revolutions per minute – steel on steel. Only the very hardest of components can take the strain. But how is that hardness achieved?

Read more