CASE STUDY Power Generation

How we protect the environment and DNA samples from around the world

Posted on November 12, 2020

mtu Kinetic PowerPack for world's leading institutes and organizations in genomics and computational biology ensuring uninterruptable power to overcome some of humanity's most significant challenges.
Details

Who

Wellcome Trust Sanger Genome Campus

What

Dynamic UPS

Why

To establish energy saving and reduce carbon emissions

Where

Hinxton, England

Situation

The Wellcome Trust Sanger Genome Campus in Hinxton (England) is home to some of the world's leading institutes in genomics and computational biology, committed to delivering life-changing science with the reach, scale, and imagination to overcome some of humanity's most significant challenges.

Their IT infrastructure is one of the most advanced in the world and contains data research from every corner of the world that must be accessible at all times. The key challenges in this project were retaining the beautiful natural scenery and completion of the scheme with a reduced carbon footprint.

Solution

To achieve the latter, Campus Facilities Management and staff have worked together to establish energy saving and recycling initiatives and like so, strive to reduce carbon emissions. As part of this aim, they have gained ISO 14001 accreditation. As managing energy costs is obviously good practice, businesses try to predict the events and reduce energy consumption during these periods.

But perhaps more importantly, the battery-free smaller footprint solution, now branded as mtu Kinetic PowerPack after Rolls-Royce acquired the former Kinolt S.A., includes the facility to participate in peak shaving schemes, choosing a self-evident one. Although peak shaving is a secondary function and is immediately aborted when the input mains fall out of tolerance, spare capacity in the dynamic UPS output can be utilized to reduce total site demand from the utility supplier.

Result

Two dynamic UPS systems were designed, built, and installed in three months, supervised by Richard Eve, our Technical Manager in the UK. Each dynamic UPS unit, equipped with top-of-the-line engine exhaust silencers and noise control equipment, is housed in a ground floor purpose built acoustic enclosure rated at 65dBA @1m in conditioning mode and 75dBA @1m in the engine running mode.

The controls for each system are housed in a separate switch room enclosure on the first floor, which also contains a close fit 11kV substation with a Schneider ringmaster and ANAN transformer. An underbelly fuel tank located underneath the D-UPS supports the unit for 48 hours of operation of the engine at a 75% load. All of the above is now supported and serviced by our service personnel. The units are remotely monitored, and any incident will be noticed by Rolls-Royce’s unique HMI, KS® VISION.

Looking for Dynamic UPS related sales or service partners?

Power Generation

mtu safeguards continuous emergency operation at Kårstø natural gas processing plant

The Norwegian natural gas processing plant at Kårstø has been equipped with a new emergency power system as part of a long-term expansion project. During any future power outages, five mtu gensets powered by Type 16V 4000 G63 engines will be in place to supply the energy for essential production processes — and, thanks to special acoustic technology, they will do their job more quietly than ever.

Read more

Power Generation

Biogas Plant in Löningen with mtu engines in long-term trial guaranteed prices for operators of a combined heat and power system

In 2008, GF-Bio-Energie Hasetal GmbH in Löningen, Germany, replaced their dualfuel engines with mtu Biogas powered Otto cycle en-gines. To maximize cost effectiveness, the company aims for high performance from each combined heat and power system. In light of the experience gathered with the 350-kilowatt engines, the company was thus very interested to try the new megawatt engine in the 4000 Series. Since 2009, this machine has been the “best horse in the paddock” at Löningen.

Read more

Power Generation

More operational flexibility and cost savings for regional medical center with new generator sets and paralleling switchgear

Recognized as the region’s leading healthcare provider, The Medical Center of Columbus Regional Healthcare System is a 400-bed hospital that offers a comprehensive menu of medical services. Like all healthcare facilities, The Medical Center relies on emergency standby generators to ensure uninterrupted electrical power during utility outages. However, also like many established healthcare facilities, the hospital’s backup system was an aging collection of standby generators that had been added over the years as the hospital grew. The generators were still adequate to power critical loads during utility outages, but they lacked the capacity to handle the hospital’s total electrical load (including HVAC) and allow load management practices.