PRESS RELEASE Power Generation

Rolls-Royce supplies power solutions for Space DC’s first Indonesian green focused data centre facility

Posted on November 17, 2020, Images by fernandogomulya.com; Rolls-Royce

SpaceDC officially launched its new ID01 25.45MW data centre campus with Rolls-Royce technology beginning of November 2020. It is the first green focused data centre in Indonesia.

Images [1 Files, 928 KB]

  • Rolls-Royce delivered 3 mtu gas and diesel systems for SpaceDC data centre in Jakarta 
  • mtu gensets are specifically designed for efficiency and hot and humid conditions 
  • Common goal: Lowering the environmental impact of data centres

SpaceDC officially launched its new ID01 25.45MW data centre campus with Rolls-Royce technology beginning of November 2020. It is the first green focused data centre in Indonesia. With innovative design and infrastructure SpaceDC enables a power usage effectiveness (PUE) of 1.3, which is changing the industry’s approach to carbon footprint. Three mtu gas and diesel systems from Rolls-Royce with the latest exhaust aftertreatment technology provide efficient and clean base load and emergency power as well as cooling.

“There is growing demand for local data centres in Southeast Asia, even more since the Covid-19 crisis”, says Darren Hawkins, CEO of SpaceDC. “With the trend of decarbonization new concepts of power supply for data centres are at the forefront.” SpaceDC is a data centre provider who aims to lower the environmental impact of data centres. “This company philosophy fits very well with Rolls-Royce's goal of continuously enhancing the eco-friendliness of our drive and energy systems and bringing them closer to CO2 neutrality,” explains Andreas Görtz, Vice President Power Generation at Rolls-Royce Power Systems.

For the JAK2 facility in the SpaceDC campus in Jakarta, Rolls-Royce supplied three containerized gas and diesel systems. The diesel systems, which secure the emergency power supply of the data centre, comprise two mtu 20V4000 DS3300 gensets in a 40 ft container with SCR systems to reduce emissions.

“Reliable backup power is the lifeblood for any data centre – and it is absolutely fundamental in creating a world class facility,” said Darren Hawkins. “In designing our JAK2 data centre, we selected Rolls-Royce, with its mtu products, as our partner because they provide the best in market technology and power efficiency for this data centre, which is aligned with our vision of meeting international standards as part of the overall value proposition to our customers in the region and beyond.”

A 20-cylinder mtu Series 4000L64 FNER gas genset in a 40ft container is installed as CHP (Combined Heat and Power) application with a total efficiency of above 90%. The system will provide baseload electricity and cooling via an absorption chiller utilising the exhaust gas heat to provide cooling. The mtu gas systems offer best in class power density and have been designed specifically to withstand hot and humid conditions. This is especially crucial for the facility in Jakarta where the climate is tropical almost year-round. The mtu power solutions offer an extended Time Between Overhaul (TBO) of 84,000 hours, requiring less maintenance and overhaul intervals for maximum productivity and reliability.

“Deploying generators in a tropical environment like Indonesia comes with a unique set of challenges, especially for a data centre environment where uptime is absolutely critical. We’re proud that our Series 4000 generator sets will help SpaceDC meet the special demands of the location and ensure the highest levels of reliability for their customers,” said Andreas Görtz.

“Working with SpaceDC, we’ve seen great synergy in developing complete power generation solutions that are market-leading in terms of efficiency and reliability. And we are proud that they chose us as a partner to support them with our sustainability service and backup power”, said Waluyanto Sukajat, Acting Managing Director, PT. MTU Indonesia.

About SpaceDC

SpaceDC is creating state-of-the-art data centres to help businesses grow in Southeast Asia’s fast-moving digital markets. Headquartered in Singapore, SpaceDC is applying over 60 years of combined leadership experience to create a network of top-of-the-line data centre campuses in Southeast Asia’s key regional cities. The campuses are strategically located to tap the cities’ natural resources and maximize accessibility. They feature multiple layers of security, dark fiber connectivity and very low PUEs to ensure business critical data is always secure and accessible. SpaceDC offers a collaborative partnership that enables to hyperscale on a long-term lease.

About Rolls-Royce Holdings plc

  1. Rolls-Royce pioneers cutting-edge technologies that deliver clean, safe and competitive solutions to meet our planet’s vital power needs.
  2. Rolls-Royce Power Systems is headquartered in Friedrichshafen in southern Germany and employs around 10,000 people. The product portfolio includes mtu-brand high-speed engines and propulsion systems for ships, power generation, heavy land, rail and defence vehicles and for the oil and gas industry as well as diesel and gas systems and battery containers for mission critical, standby and continuous power, combined generation of heat and power, and microgrids. Medium-speed engines from Bergen power ships and power generation applications.
  3. Rolls-Royce has customers in more than 150 countries, comprising more than 400 airlines and leasing customers, 160 armed forces, 70 navies, and more than 5,000 power and nuclear customers.
  4. Annual underlying revenue was £15.45 billion in 2019, around half of which came from the provision of aftermarket services.
  5. In 2019, Rolls-Royce invested £1.46 billion on research and development. We also support a global network of 29 University Technology Centres, which position Rolls-Royce engineers at the forefront of scientific research.
Silke Rockenstein Spokeswoman Trade Media
Phone:
+49 7541 90 7740
E-mail: