PRESS RELEASE Power Generation

Rolls-Royce supplies eight battery containers for power grid stabilization and power trading to VISPIRON

Posted on November 10, 2022

Images [2 Files, 6 MB]

Videos [1 Files, 58 MB]

  • Battery storage systems from Rolls-Royce make an important contribution to the success of the energy transition
  • VISPIRON uses mtu EnergyPacks in solar parks in Germany

Rolls-Royce has already delivered six of a total of eight mtu EnergyPacks to VISPIRON, the southern German provider of sustainable mobility and energy solutions. The battery storage systems have largely been commissioned in solar parks in Bavaria and Thuringia in Germany and are used for so-called intraday trading, i.e. the short-term purchase and sale of electricity delivered on the same day.  

Intraday trading is particularly important for absorbing unpredictable changes in electricity production and demand caused by the volatile feed-in of renewable energy sources such as solar and wind. “With regard to increasingly volatile electricity markets, battery storage can be used to profitably market storage capacity while having a stabilizing effect on our power grids,” explained Florian Schönberger, CTO of VISPIRON ENERGY GmbH & Co. KG.  

One of the decisive factors for VISPIRON to cooperate with the business unit Power Systems of Rolls-Royce was that the mtu EnergyPacks are fully integrable, modular systems, which are available with power ratings from 60 kVA to 2,000 kVA as well as a storage capacity from 70 kWh to 2,200 kWh and are characterized by high availability.  

As marketer of the battery storage systems and green power supplier, SEtrade GmbH, a member of the VISPIRON Group, uses the virtual power plant in combination with an autotrading system to react to price fluctuations on the stock exchange in real time.

“We see a growing market in the VISPIRON business model and in our storage products and are pleased that together we can make a relevant contribution to grid and supply stability and thus actively contribute to the energy transition,” said Andreas Görtz, President Sustainable Power Solutions at Rolls-Royce Power Systems.

Rolls-Royce produces its battery systems at its own plant in Ruhstorf, Bavaria. The products are offered as 20- and as 40-foot containers or as compact versions (slightly smaller than 10 feet) under the mtu brand. They are scalable, so they can be flexibly adapted to customers’ performance and capacity requirements. In addition to the lithium-ion battery modules, the mtu EnergyPacks include electronic controls, inverters and cooling equipment, making them a complete storage solution. Battery storage is a core component of microgrids, but is also integrated into solar parks for grid stabilization, for example, or serves the charging infrastructure of e-mobility. More than 100 mtu energy packs are already in use worldwide.

The VISPIRON Group from Munich develops, plans, builds and operates solar parks, energy storage, charging infrastructure and shared mobility as well as smart energy and mobility solutions. Further information about VISPIRON: https://www.vispiron.com.


About Rolls-Royce Holdings plc

  1. Rolls-Royce pioneers the power that matters to connect, power and protect society. We have pledged to achieve net zero greenhouse gas emissions in our operations by 2030 (excluding product testing) and joined the UN Race to Zero campaign in 2020, affirming our ambition to play a fundamental role in enabling the sectors in which we operate achieve net zero carbon by 2050.
  2. Rolls-Royce Power Systems is headquartered in Friedrichshafen in southern Germany and employs around 9,000 people. The product portfolio includes mtu-brand high-speed engines and propulsion systems for ships, power generation, heavy land, rail and defence vehicles and for the oil and gas industry as well as diesel and gas systems and battery containers for mission critical, standby and continuous power, combined generation of heat and power, and microgrids and is intensively engaged in the development of climate-neutral solutions.
  3. Rolls-Royce has customers in more than 150 countries, comprising more than 400 airlines and leasing customers, 160 armed forces and navies, and more than 5,000 power and nuclear customers.
  4. Annual underlying revenue was £10.95 billion in 2021, underlying operating profit was £414m and we invested £1.18 billion on research and development. We also support a global network of 28 University Technology Centres, which position Rolls-Royce engineers at the forefront of scientific research.
  5. Rolls-Royce Holdings plc is a publicly traded company (LSE:RR., ADR: RYCEY, LEI: 213800EC7997ZBLZJH69).

Contact

Silke Rockenstein Spokeswoman Trade Media
Phone:
+49 7541 90 7740
E-mail::