PRESS RELEASE Naval Solutions

Rolls-Royce to supply mtu generator sets for U.S. Navy frigate program

Posted on May 11, 2021

Images [2 Files, 830 KB]

  • New frigate warship to serve as the next generation of small surface combatants for the U.S. Navy
  • mtu naval generator sets to be key component of propulsion and on-board power generation

Rolls-Royce has been selected to supply its mtu naval generator sets for phase one of the U.S. Navy’s Constellation (FFG-62) class frigate program, previously known as the FFG(X) program. Rolls-Royce has received a contract for the first shipset to provide four mtu naval generator sets, each rated at 3000 kWe at 1800 rpm.

The Navy Constellation (FFG-62) Class Frigate is a multi-mission warship designed for operation in littoral and blue water environments to conduct air, anti-submarine, surface and electronic warfare, in addition to information operations. The generator sets are based on the mtu 20V 4000 M53B engine and provide a total power output of 12 MW for propulsion and on-board power supply.

Adam Wood, Director, Government Sales North America at Rolls-Royce business unit Power Systems, said: “We’re very proud that Fincantieri Marinette Marine has placed its trust in our mtu naval generator sets for this important program. We have a legacy of strong support for our partners in both the U.S. Navy and the U.S. Coast Guard, and we are honored to be selected for FFG-62. There is no doubt that our systems will perform to the high expectations and unique demands of the U.S. Navy Constellation Class.”

The flexible design engineering of the frigate’s CODLAG propulsion system will allow for energy-efficient diesel power generation for propulsion at normal cruising speeds with extended range, while enhancing anti-submarine capability in its extremely quiet diesel-electric configuration. When completed, the lead ship will be nearly 500 feet in length, accommodate up to 200 Sailors and be capable of sustained speeds of more than 26 knots.

Fincantieri Marinette Marine (FMM) of Marinette, Wisconsin (USA), was awarded the build contract for the project, which includes the design and construction of the lead ship and the option to build up to 10 ships in total for phase one. A potential planned second phase would include another 10 ships.

Construction on the first ship is expected to begin later this year.

About Rolls-Royce Holdings plc

  1. Rolls-Royce pioneers the power that matters to connect, power and protect society. We have pledged to achieve net zero greenhouse gas emissions in our operations by 2030 [excluding product testing] and joined the UN Race to Zero campaign in 2020, affirming our ambition to play a fundamental role in enabling the sectors in which we operate achieve net zero carbon by 2050.
  2. Rolls-Royce Power Systems is headquartered in Friedrichshafen in southern Germany and employs around 9,000 people. The product portfolio includes mtu-brand high-speed engines and propulsion systems for ships, power generation, heavy land, rail and defence vehicles and for the oil and gas industry as well as diesel and gas systems and battery containers for mission critical, standby and continuous power, combined generation of heat and power, and microgrids.
  3. Rolls-Royce has customers in more than 150 countries, comprising more than 400 airlines and leasing customers, 160 armed forces and navies, and more than 5,000 power and nuclear customers.
  4. Annual underlying revenue was £11.76 billion in 2020 and we invested £1.25 billion on research and development. We also support a global network of 28 University Technology Centres, which position Rolls-Royce engineers at the forefront of scientific research.

Contacts

Jennifer Riley Spokeswoman North- and Latin America
Phone:
+1 248 560 8488
E-mail: