mtu engines from Rolls-Royce provide emergency power on offshore wind platforms in the UK
Posted on July 01, 2025
- Four engines from the mtu Series 4000 provide emergency power for two converter platforms
- Norfolk wind farm will generate electricity for demand from more than four million households
Rolls-Royce has received a second order from Eureka Pumps AS to supply mtu Series 4000 engines to power emergency power generators for the Norfolk Offshore Wind Farm on the east coast of the United Kingdom. Rolls-Royce will thus supply a total of four mtu engines for the first and second phases of the large wind farm, which is operated by energy supplier RWE. The engines will be installed on two converter platforms at sea and onshore, which are the heart of the offshore grid connection: they ensure that the electricity generated at sea can be fed into the power grid. With a total capacity of 4.2 GW, the wind farm is expected to generate electricity for more than four million households during the course of this decade. It is located 50 to 80 kilometers off the east coast of the UK.
The emergency power generators based on 20-cylinder mtu Series 4000 P63 engines, each with an output of 2,600 kWe, ensure that the power supply on the converter platforms remains stable even if the main power supply fails. They also ensure that control and monitoring systems continue to operate, that the infrastructure of the service crew quarters is maintained, and that lighting and other safety-critical systems do not fail. They also supply power for cooling and ventilation of important system components to prevent damage from overheating. In extreme cases, the emergency power generators enable the systems to be shut down and restarted in a controlled manner.
“The engines have to be extremely reliable because they are the piece of the puzzle that matters when it comes down to it,” explained Detlev Köster, Sales Manager in the Offshore business at Rolls-Royce Power Systems. “We are delighted that Eureka Pumps is continuing to rely on our products in project phase 2.”
Rolls-Royce secures critical infrastructure worldwide in line with its strategy: The company offers mtu emergency power solutions based on diesel and gas generators as well as dynamic uninterruptible power systems (UPS). In addition to offshore platforms, these include data centers, industrial plants, airports, hospitals, power plants, and numerous other facilities that require an uninterruptible power supply.
About Rolls-Royce Holdings plc
- Rolls-Royce is a force for progress; powering, protecting and connecting people everywhere. Our products and service packages help our customers meet the growing need for power across multiple industries; enable governments to equip their armed forces with the power required to protect their citizens; and connect people, societies, cultures and economies together.
- Rolls-Royce has a local presence in 47 countries and customers in over a hundred more, including airlines and aircraft leasing companies, armed forces and navies, and marine and industrial customers.
- Through our multi-year transformation programme, we are building a high-performing, competitive, resilient and growing Rolls-Royce. We are building the financial capacity and agility to allow us to successfully develop and deliver the products that will support our customers through the energy transition.
- Annual underlying revenue was £20.1 billion in 2025, and underlying operating profit was £3.46 billion.
- Rolls-Royce Holdings plc is a publicly traded company (LSE: RR., ADR: RYCEY, LEI: 213800EC7997ZBLZJH69).
- Rolls-Royce Power Systems is headquartered in Friedrichshafen in southern Germany and employs more than 10,350 people. The product portfolio includes mtu-brand high-speed engines and propulsion systems for ships, heavy land, rail and defence vehicles and for the oil and gas industry. The portfolio also includes diesel and gas systems and battery containers for mission critical, standby and continuous power, combined generation of heat and power, and microgrids. With its climate friendly technologies, Rolls-Royce Power Systems is helping to drive the energy transition.
Contact
| Phone: |
+49 7541 90 7740
|
| E-mail: |