STORY Yacht

Introducing Veloce, the world's fastest aluminum yacht

Posted on June 17, 2021 by Kerstin Hansmann

"Veloce" is to become the world's fastest aluminium yacht in its category. Three mtu engines of the type 16V2000M96L are to bring the yacht to the record speed of over 50 knots.
Flevoland, Netherlands
“Veloce” is Italian for “fast”. Dutch yacht builder Vanquish could not have given its new 35-meter yacht a more fitting name – because it is set to become the world's fastest aluminum yacht in its category.

Normally, yachts of this size can manage an average maximum speed of 35 – 45 knots. But not Veloce, whose three mtu 16V2000M96L engines will each deliver 1,939 kW (2,600 PS) of oomph to power the yacht to well over 50 knots (93 km per hour). This will make her the fastest diesel-powered aluminum yacht over 30 meters in length. How that works? Veloce has a so-called surface drive. Here, the propeller is only half under water and its inclination is adjustable. This reduces water resistance - and increases speed. 

Erik van Prooijen, Project Manager at Vanquish Yachts, affectionately refers to the yacht as a “speed machine”.

“This crazy fast family cruiser combines speed and comfort in a unique way. In Rolls-Royce we have found an outstanding partner for this extraordinary project. We have full confidence in mtu engines and look forward to a great partnership.”

Erik van Prooijen - Project Manager at Vanquish Yachts

The game changing VQ115 Veloce is made entirely of aluminum, aiding speed as aluminum yachts are much lighter than steel craft. The vessel can achieve an impressive range of up to 500
nautical miles when powered by two engines and contains an extra fuel tank for
cruising at 15 knots.

"We can hardly wait to see the yacht on the water. We're proud that this impressive record-breaking yacht is to be powered by mtu engines.”

Wouter Hoek - Senior Sales Manager Marine at Rolls-Royce

The yacht is scheduled for delivery to its owner at the end of June 2022. We are already curious when and where he will chase her over the 50-knot threshold!

 

Yacht

Quartet of innovations: The new integrated mtu yacht systems

by Rebecca Lorenz

With an integrated bridge, an mtu powerhouse as its engine, and an efficient POD system, Rolls-Royce is setting new standards for performance, safety, and sustainability on board yachts.

Read more

Commercial Marine

Green methanol for mtu marine engines

by Lucie Maluck

What makes methanol such an interesting alternative for shipping? And what challenges await the Rolls-Royce engineers who are developing mtu engines for this fuel?

Read more

Yacht

London to Monaco to save the seas

by Wolfgang Boller

The 8-strong pedaling team mtu Power4Seas is cycling all the way from London to Monaco to raise funds for the environmental organization Blue Marine Foundation.

Read more

Yacht

Speed, comfort, efficiency, locally emission-free - mtu Hybrid PropulsionPack

by Vanessa Bösch

Rolls-Royce's mtu Hybrid PropulsionPack offers more than one way to design hybrid propulsion for ships. Adapted to the customer's wishes, it can not only ensure lower emission levels, but also silence on board - whether in the harbor or at anchor.