PRESS RELEASE Commercial Marine

Gas engines with gas protection: Rolls-Royce supplies innovative propulsion system for new multi-purpose vessels in the North and Baltic Seas

Posted on March 31, 2020

Images [1 Files, 2 MB]

  • Gas protection enables vessels to circulate in explosive and toxic environments

  • Rolls-Royce applies decades of experience in medium-speed gas engines

Rolls-Royce is supplying the gas-shielded propulsion system for two new multi-purpose vessels to keep them operational even under difficult conditions. In future, the 95-m special ships will be called out on the North and Baltic Seas to deal with accidents, fires or unable-to-maneuver vessels. They are being built for the German Federal Waterway and Shipping Administration by Abeking & Rasmussen, the ship and yacht yard based in Lemwerder, Lower Saxony. The vessels are replacing their predecessors, the Scharhörn and Mellum, after 46 and 36 years of service respectively. The ship technology division of the Federal Waterways Engineering and Research Institute was commissioned with planning, design and tendering and now with construction management.

Specially certified engine configuration enables use in explosive environments 

The two ships are powered by gas-electric propulsion systems based on four medium-speed Bergen B36:45L6AG units from Rolls-Royce, each delivering 3,600 kW. Rolls-Royce is not only engine and generator supplier, but provider of a special solution in the form of the gas protection specially developed to allow the engines to remain operational even if, for example, the ambient air has been contaminated with explosive gases following a gas tanker accident. "Obviously the engines are there to burn gas, but if gas gets into the combustion chamber in an uncontrolled way via the intake air, the engine will become unmanageable," explained Rolls-Royce project manager Christian Prinz. With the system Rolls-Royce has developed, the engine power output is adjusted in relation to the amount of gas in the intake air. In short, the more gas there is in the intake air of the engine, the less gas fuel is fed to the engine via the gas control valves. If the gas volume is too high, special quick-acting flaps shut off the intake of gas and air and the engine comes to a stop. 

Combination of experience and new special-purpose technology 

"With these ships, we’ve combined the decades of experience we have under our belt in the field of medium-speed gas engines from Rolls-Royce with our highly specialized gas protection expertise to create an effective solution for our customer," said Knut Müller, Vice President Marine at Rolls-Royce. Indeed, Rolls-Royce is the only manufacturer worldwide able to supply such powerful engines with gas protection and the relevant certification. They have already proven their worth in sea rescue cruisers, pollution control vessels and most recently in the Nordic, the North Sea emergency tug. Rolls-Royce has been supplying medium-speed gas engines for over 20 years. 

"Rolls-Royce was the only manufacturer worldwide able to utilize its long-standing experience in this specialized field and develop gas protection for straightforward gas engines, all in line with our schedule requirements and backed up by the relevant feasibility study," pointed out Carsten S. Wibel, head of Abeking & Rasmussen Special Vessels GmbH.

The two predecessor vessels – the Scharhörn and the Mellum – were likewise powered with mtu-brand engines from Rolls-Royce. "The customer was impressed not only by mtu propulsion, but by the quality of the service we provided, and that swayed his decision in our favor," said Jörg Fischer-Felsberg, Director of Sales and Service for mtu products in Germany. 

In the event of an emergency, the new ships, capable of speeds over 15 knots, will be at the accident scene in no more than  two hours. Equipped with emergency towing capabilities with 145 tons bollard pull, chemical tanks, an explosion-proof safety and container cargo hold, as well as oil collection equipment such as skimmers, oil-holding tanks and a separation room, they are able to accomplish the most challenging missions. Not only the engines, but the entire ship is gas-protected. If it enters a dangerous zone in which there are flammable or health-endangering substances in the air, the crew must switch the ship to gas-protection mode, meaning that windows and doors must be sealed gas-tight. This creates a citadel into which clean air is pumped. The resulting overpressure ensures that no more toxic  air can enter. 

That gas engines are being used in this project is owing to a German government directive that requires a massive reduction in CO2 emissions from governmental vessels. Enak Ferlemann, Parliamentary State Secretary to the Federal Minister of Transport and Digital Infrastructure, said, "With the new LNG-powered ships that also carry the Blue Angel environmental certificate, we’re simultaneously ensuring top safety and top environmental standards in high-tech shipbuilding.”

By the end of 2020, a decision is to be made as to whether a third, identical vessel should be built. The two ordered so far are to go into service in 2023 and 2024.

Press photos are available for download from www.rrpowersystems.com/press   

Read more about Rolls-Royce power generation based on medium-speed engines at 
www.rolls-royce.com/bergen

About Rolls-Royce Holdings plc

  1. Rolls-Royce pioneers cutting-edge technologies that deliver clean, safe and competitive solutions to meet our planet’s vital power needs.

  2. Rolls-Royce Power Systems is headquartered in Friedrichshafen in southern Germany and employs more than 10,000 people. The product portfolio includes mtu-brand high-speed engines and propulsion systems for ships, power generation, heavy land, rail and defence vehicles and for the oil and gas industry as well as diesel and gas systems and battery containers for mission critical, standby and continuous power, combined generation of heat and power, and microgrids. Medium-speed engines from Bergen power ships and power generation applications.

  3. Rolls-Royce has customers in more than 150 countries, comprising more than 400 airlines and leasing customers, 160 armed forces, 70 navies, and more than 5,000 power and nuclear customers.

  4. Annual underlying revenue was £15.3 billion in 2019, around half of which came from the provision of aftermarket services. 

  5. In 2019, Rolls-Royce invested £1.45 billion on research and development. We also support a global network of 29 University Technology Centres, which position Rolls-Royce engineers at the forefront of scientific research.

  6. The Group has a strong commitment to apprentice and graduate recruitment and to further developing employee skills. 

Wolfgang Boller Spokesman Regional and Business Media
Phone:
+49 7541 90 2159
E-mail: