Rolls-Royce strengthens marine connectivity with Majestic Fast Ferry
Posted on May 09, 2024
Rolls-Royce has signed a Memorandum of Understanding (MOU) in Singapore, to further strengthen its partnership with Majestic Fast Ferry Pte Ltd in enabling clean, energy-efficient sailings for its current fleet of 11 ferries, fitted with mtu propulsion systems.
The event also commemorated the ferry operator’s 100th mtu engine purchased since 2016 from Rolls-Royce Solutions Asia, a subsidiary of the Power Systems division of Rolls-Royce. Majestic Fast Ferry uses mtu Series 2000 engines, with the 100th unit being the 16V 2000 M72 with a power output of 1,440 kW.
The MOU was signed by President of Global Markets Rolls-Royce Power Systems and Managing Director of Rolls-Royce Solutions Asia, Giovanni Spadaro and Managing Director of Majestic Fast Ferry, Max Tan and witnessed by President – Power Systems, Rolls-Royce, Jörg Stratmann and Board Director at Majestic Fast Ferry, Zhang Mao Xin.
The signing of the MOU reaffirms the longstanding ties and joint commitment by both companies to strengthen marine connectivity, whilst looking into alternative fuel sources to enable a greener maritime industry, according to the Power Systems strategy.
Spadaro says, “In a world where challenges are complex and interconnected and resources limited, collaboration becomes imperative. Through this MOU, we pledge to leverage our respective strengths, resources, and networks to drive innovation, foster sustainable development, and create positive impact in our communities and beyond.”
Under the MOU, Rolls-Royce will continue partnering Majestic Fast Ferry to ensure ferry services are as sustainable as possible, including the use of engines and propulsion solutions that are able to run on hybrid and renewable fuels such as Hydrotreated Vegetable Oil (HVO). This trust towards executing viable green solutions for Majestic Fast Ferry’s fleet is based on Rolls-Royce’s “reliability, fuel efficiency and performance over the number of years that made us a loyal client,” said Tan and added “Majestic Fast Ferry is currently 30% more fuel-efficient compared to our competitors. We are proud of this progress, as we continue to reduce emissions in our operations. We will certainly continue to assess and review our fuel strategy and ensure we remain at the forefront of efficiency and decarbonization.”
Changing the face of ferry travel on the Singapore Strait and beyond
Majestic Fast Ferry started with one ferry in December 2014, growing to 1.3 million passengers in 2023. As one of the youngest leading operators coming out of Singapore in a highly competitive ferry transportation industry, Majestic Fast Ferry sought to remain bold and innovative in capturing growing markets.
This led to the purchase of its first mtu engines in 2016, which delivered the best weight ratio of its class. Having Singapore and Indonesia offices for mtu engines also meant Majestic Fast Ferry could enjoy instant support and quick response-resolution times.
In 2023, as Batam grew in popularity for domestic travel, Majestic Fast Ferry started using mtu-powered vessels for its high-speed catamaran service, making it possible to serve the route more efficiently in comparison to using slower, traditional monohulled vessels.
“With an mtu-powered vessel, it is possible to carry almost double the amount of passengers compared to our previous ferry. On top of that, the mtu-powered vessels are using the same amount of fuel as before but achieving a much faster speed,” said Tan.
Director of Marine APAC, Rolls-Royce Power Systems, Chew Xiang Yu said, “The recognition from Majestic Fast Ferry is a testament of our APAC team's dedication to customer service. At Rolls-Royce, we stand ready to partner with our customers, offering unwavering commitment throughout their journey.
Five decades to the community and industry
The Memorandum of Understanding was signed on the same day that Rolls-Royce Solutions Asia celebrated its 50th anniversary in Singapore. Serving over 30 countries across Asia, the company is supported by a dedicated team of approximately 300 employees locally, providing service solutions that play pivotal roles in the industrial, naval, governmental, commercial marine, and power generation sectors.
About Rolls-Royce Holdings plc
- Rolls-Royce is a force for progress; powering, protecting and connecting people everywhere. Our products and service packages help our customers meet the growing need for power across multiple industries; enable governments to equip their armed forces with the power required to protect their citizens; and connect people, societies, cultures and economies together.
- Rolls-Royce has a local presence in 47 countries and customers in over a hundred more, including airlines and aircraft leasing companies, armed forces and navies, and marine and industrial customers.
- Through our multi-year transformation programme, we are building a high-performing, competitive, resilient and growing Rolls-Royce. We are building the financial capacity and agility to allow us to successfully develop and deliver the products that will support our customers through the energy transition.
- Annual underlying revenue was £20.1 billion in 2025, and underlying operating profit was £3.46 billion.
- Rolls-Royce Holdings plc is a publicly traded company (LSE: RR., ADR: RYCEY, LEI: 213800EC7997ZBLZJH69).
- Rolls-Royce Power Systems is headquartered in Friedrichshafen in southern Germany and employs more than 10,350 people. The product portfolio includes mtu-brand high-speed engines and propulsion systems for ships, heavy land, rail and defence vehicles and for the oil and gas industry. The portfolio also includes diesel and gas systems and battery containers for mission critical, standby and continuous power, combined generation of heat and power, and microgrids. With its climate friendly technologies, Rolls-Royce Power Systems is helping to drive the energy transition.
Contact
| Phone: |
+49 7541 90 2159
|
| E-mail: |