PRESS RELEASE Land Defense

Rolls-Royce unveils the mtu PowerPack Xelerate: An integrated hybrid propulsion system for land forces

Posted on June 15, 2026

Images [2 Files, 5 MB]

  • World premiere: Rolls-Royce Power Systems is exhibiting the hybrid powerpack announced in March for the first time at Eurosatory under the name mtu PowerPack Xelerate
  • Over 1,400 kW: integrated hybrid drive based on the mtu 10V 199 engine and the eLSG 5000 electrified transmission from ZF
  • Rolls-Royce Power Systems is responsible for the integration, system architecture and overall design of the powertrain
  • A step towards an integrated system solution for heavy tracked vehicles with clear operational advantages
  • Efficient and robust powertrain architecture with European industrial value creation

Rolls-Royce Power Systems will be showcasing its mtu PowerPack Xelerate parallel hybrid system for the first time at Eurosatory 2026. This brings the system, announced in March, to life: the engine, transmission and electrical power system form a highly integrated complete system. The hybrid powerpack combines the mtu 10V 199 engine with ZF’s eLSG 5000 electrified manual gearbox and achieves a system output of over 1,400 kW. The combination of a high-performance diesel engine, an electrified transmission and a highly integrated system architecture forms the basis for a new generation of powerful and energy-efficient powertrains for military tracked vehicles. This strengthens Rolls-Royce Power Systems’ position as a provider of integrated system solutions and boosts European industrial value creation in the field of military mobility.

The new mtu PowerPack Xelerate significantly expands the vehicle’s capabilities and enhances its operational effectiveness. It makes the vehicle more agile and directs power to where it is needed in any given situation. The high power density and electrified components allow for greater flexibility in vehicle integration. This has a positive effect on the vehicle’s architecture and makes it possible to reduce the total weight of tracked vehicles to the level of the MLC 60 class – which corresponds to around 54 tonnes. At the same time, the drivetrain can be controlled entirely electronically (‘drive-by-wire’) and is thus ready for future vehicle concepts, including unmanned ones.

Andreas Görtz, President of the Mobile & Sustainable Business Unit at Rolls-Royce Power Systems, said at the launch on Monday 15 June at Eurosatory in Paris:“With the mtu PowerPack Xelerate, we are launching an integrated propulsion system that effectively combines the growing demands for energy, power and efficiency. It embodies a clear systems-based approach – featuring intelligent hybridisation, high power density and proven robustness.” 

The unveiling of the hybrid powerpack was attended by high-ranking representatives from the worlds of politics and industry. Alongside Andreas Görtz and Dr Andreas Strecker, Chief Financial Officer at Rolls-Royce Power Systems, Jens Lehmann, Member of the German Bundestag, also attended the presentation at Eurosatory.

More power and energy for the battlefield of the future

Modern land forces are undergoing a transformation: alongside conventional propulsion power, there is a growing demand for electrical energy to power sensors, communications and protection systems. At the same time, efficiency, range and signature reduction are becoming increasingly important.

The mtu PowerPack Xelerate addresses these requirements comprehensively: for armed forces, this means greater operational readiness, additional power for complex on-board systems and a propulsion solution that can be flexibly integrated into different vehicle types. At the same time, the systematic approach simplifies operation and maintenance and helps to make logistical processes more efficient.

From innovation to application

With the mtu PowerPack Xelerate, Rolls-Royce Power Systems is taking the next step towards operational readiness. The hybrid powerpack now unveiled builds on current development work (such as the MGCS programme) and takes the technology from the concept phase into a tangible, integrated system solution that will also be of great significance for future programmes. The first prototypes are expected later this decade, with the prospect of series production in future platforms from the 2030s onwards.

Further information on Rolls-Royce Power Systems’ presence at Eurosatory can be found here. 

Visit us from 15 to 19 June 2026 in Paris at our exhibition stand in Hall 6, Stand J335.

About Rolls-Royce Holdings plc

  1. Rolls-Royce is a force for progress; powering, protecting and connecting people everywhere. Our products and service packages help our customers meet the growing need for power across multiple industries; enable governments to equip their armed forces with the power required to protect their citizens; and connect people, societies, cultures and economies together.
  2. Rolls-Royce has a local presence in 47 countries and customers in over a hundred more, including airlines and aircraft leasing companies, armed forces and navies, and marine and industrial customers.
  3. Through our multi-year transformation programme, we are building a high-performing, competitive, resilient and growing Rolls-Royce. We are building the financial capacity and agility to allow us to successfully develop and deliver the products that will support our customers through the energy transition.
  4. Annual underlying revenue was £20.1 billion in 2025, and underlying operating profit was £3.46 billion.
  5. Rolls-Royce Holdings plc is a publicly traded company (LSE: RR., ADR: RYCEY, LEI: 213800EC7997ZBLZJH69).
  6. Rolls-Royce Power Systems is headquartered in Friedrichshafen in southern Germany and employs more than 10,350 people. The product portfolio includes mtu-brand high-speed engines and propulsion systems for ships, heavy land, rail and defence vehicles and for the oil and gas industry. The portfolio also includes diesel and gas systems and battery containers for mission critical, standby and continuous power, combined generation of heat and power, and microgrids. With its climate friendly technologies, Rolls-Royce Power Systems is helping to drive the energy transition.

www.rolls-royce.com

Contact

Johannes Jerg Head of External Communications, Press Spokesman
Phone:
+49 7541 90 8979
E-mail: